MCUXpresso SDK Documentation

Hardware requirements#

  • Mini/micro USB cable

  • MCX-N5XX-EVK Board

  • Personal Computer

Board settings#

No special settings are required.

Prepare the Demo#

  1. Connect the micro and mini USB cable between the PC host and the USB ports on the board.

  2. Open a serial terminal on PC for the serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

  5. The J20 Pin 28 (ADC0_A2) on EVK board is used to monitor the voltage.

Running the demo#

The following lines are printed to the serial terminal when the demo program is executed.

LPADC EDMA Example
Configuring LPADC...
ADC Full Range: 4096
Configuring LPADC EDMA...
Press any key to print output buffer:

0 = 3192
1 = 3192
2 = 3184
3 = 3184