Hardware requirements
Mini/micro USB cable
MCX-N9XX-EVK board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
Calling the runBootloader API to force into the ISP mode: x...
The runBootloader ISP interface is choosen from the following one:
kIspPeripheral_Auto : 0
kIspPeripheral_UsbHid : 1
kIspPeripheral_Uart : 2
kIspPeripheral_SpiSlave : 3
kIspPeripheral_I2cSlave : 4
kIspPeripheral_Can : 5
Call the runBootloader API based on the arg : xxxxxxxx...