MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • MCX-N9XX-EVK board

  • Personal Computer

Board settings#

Default MCUBoot memory layout - bootloader located in IFR region#

Region

From

To

Size

Primary slot

0x00000000

0x000FFFFF

1024kB

Secondary slot

0x00100000

0x001FFFFF

1024kB

—————-

————

————

——–

MCUboot code

0x01008000

0x0100FFFF

32kB

  • MCUBoot resides in the Bank_1 IFR_0 region to utilize flash remap feature

  • MCUBoot header size is set to 1024 bytes

  • Signing algorithm is ECDSA-P256 (TinyCrypt)

  • Write alignment is 16 bytes

  • MCUBoot is configured to use its DIRECT_XIP image handling strategy

  • Flash swapping HW feature is used for zero-overhead image swapping

  • To manually enter serial recovery mode, keep the SW2 button pressed during reset, then release it

Image signing example:

imgtool sign --key sign-ecdsa-p256-priv.pem
             --align 16
             --version 1.1
             --slot-size 0x100000
             --header-size 0x400
             --pad-header
             ota_mcuboot_basic.bin
             ota_mcuboot_basic.SIGNED.bin

Note that for the first image flashed manually together with the bootloader additional imgtool options --pad and --confirm must be used. Otherwise the bootloader would reject the image for missing data in the trailer area.

If the toolchain used for build has problems with writing the bootloader to the IFR flash region, an alternative can be to use NXP blhost utility or MCUXpresso Secure Provisioning Tool.

IMPORTANT: The CMPA region must be configured so that ROM loader boots from the IFR region. This is done by setting the BOOT_CFG.BOOT_SRC field to 0b10. This value directs the ROM loader to start execution from the IFR region where MCUboot is located. Default CMPA setup with this particular field set is attached to this example in cmpa.bin binary file. To flash this configuration together with MCUboot binary the following blhost commands can be used. Note that the board must be in the ISP mode to use the following commands:

#Erase IFR0 Bank 1 region
blhost -u 0x1FC9,0x014F -- flash-erase-region 0x01008000 32768 0

#Flash MCUboot
blhost -u 0x1FC9,0x014F -- write-memory 0x01008000 mcuboot_opensource.bin

#Flash CMPA
blhost -u 0x1FC9,0x014F -- write-memory 0x01004000 cmpa.bin

Custom configuration - Encrypted XIP#

Region

From

To

Size

MCUboot code

0x00000000

0x0003FFFF

256kB

Primary slot

0x00040000

0x0011FFFF

896kB

Secondary slot

0x00120000

0x001FFFFF

896kB

This custom build generates a project with predefined configuration to utilize Encrypted XIP mode. For more information please see Encrypted XIP and MCUboot.

Note: Default layout setup using the bootloader in IFR region limits usage of some features such as hardware accelerated mbedTLS (due size of IFR region) or encrypted XIP (due limitation of ROM). This custom configuration moves the bootloader to main flash array.

  • MCUBoot header size is set to 1024 bytes

  • Signing algorithm is ECDSA-P256

  • Write alignment is 16 bytes

  • MCUBoot is configured for Encrypted XIP mode using modified MCUBOOT_OVERWRITE_ONLY image update strategy

  • MCUboot uses ECDH-P256 to secure AES key for image encryption

  • Primary slot is encrypted by NPX module to utilize encrypted XIP

Image signing example:

imgtool sign --key sign-ecdsa-p256-priv.pem
             --align 16
             --version 1.1
             --slot-size 0xE0000
             --header-size 0x400
             --max-sectors 111
             --pad-header
             -E enc-ec256-pub.pem
             ota_mcuboot_basic.bin
             ota_mcuboot_basic.SIGNED.bin

Project building example:

The project is built using west tool. For more information please see MCUXpresso SDK documentation.

Bootloader:

west build -p always examples/ota_examples/mcuboot_opensource -b mcxn9xxevk --config debug --toolchain armgcc -Dcore_id=cm33_core0 -DCONF_FILE="examples/ota_examples/_custom_cfg/mcxn/mcuboot_opensource.conf"

OTA application:

west build -p always examples/ota_examples/ota_mcuboot_basic -b mcxn9xxevk --config debug --toolchain armgcc -Dcore_id=cm33_core0 -DCONF_FILE="examples/ota_examples/_custom_cfg/mcxn/ota_mcuboot_basic.conf"