Hardware requirements

  • Mini/micro USB cable

  • MCXW23-EVK Board

  • Personal Computer

Board settings

Short J36-7 and J18-3.

Prepare the Demo

  1. Connect a USB cable between the host PC and the EVK board J33.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

CTimer capture example Rising edge triggered and CTimer capture the edge periodically