MCUXpresso SDK Documentation

Hardware requirements#

  • Mini/micro USB cable

  • MCXW23-EVK Board

  • Personal Computer

Board settings#

No special settings are required.

Prepare the Demo#

  1. Connect a USB cable between the host PC and the EVK board J33.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

The following lines are printed to the serial terminal when the demo program is executed.

Tickless Demo example
Press SW3 to wake up the CPU

Tick count :
0
5000
CPU woken up by external interrupt
10000