Hardware requirements
- Type-C USB cable 
- MCXW72-LOC Board 
- Personal Computer 
Board settings
No special is needed.
Prepare the Demo
- Connect a USB cable between the host PC and the LOC board J3. 
- Open a serial terminal on PC for OpenSDA serial device with these settings: - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board. 
- Reset the SoC and run the project. 
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
Lpuart functional interrupt example
Board receives characters then sends them out
Now please input: