Hardware requirements#
MIMXRT700 board
Mini/micro USB cable
Personal Computer
Board settings#
Make sure the board is setup to boot from flash.
MCUBoot layout#
In all cases, the MCUBOOT bootloader reserves 256kB at the beginning of the external flash followed by 2MB slots for application.
Region |
From |
To |
Size |
|---|---|---|---|
MCUboot code |
0x28000000 |
0x2803FFFF |
256kB |
Primary slot |
0x28040000 |
0x2823FFFF |
2048kB |
Secondary slot |
0x28240000 |
0x2843FFFF |
2048kB |
MCUBoot header size is set to 1024 bytes
Signing algorithm is ECDSA-P256
Write alignment is 4 bytes
MCUBoot is configured to use its
DIRECT_XIPimage handling strategy together with FlexSPI flash remappingTo manually enter serial recovery mode, keep the user button 1 (SW5) pressed during reset, then release it
Image signing example#
imgtool sign --key sign-ecdsa-p256-priv.pem
--align 4
--version 1.1
--slot-size 0x200000
--header-size 0x400
--pad-header
ota_mcuboot_basic.bin
ota_mcuboot_basic.SIGNED.bin
Note that for the first image flashed manually together with the bootloader
additional imgtool options --pad and --confirm must be used. Otherwise
the bootloader would reject the image for missing data in the trailer area.