Hardware requirements#
Mini/micro USB cable
TWR-KM34Z75M board
Personal Computer
Board settings#
Connect J21 1-2 to use potentiometer
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
Roll the potentiometer to change the ADC value. When the example runs successfully, the following message is displayed in the terminal:
ADC16_DoAutoCalibration() Done.
The ADC16 output value is 216.
The ADC16 output value is 215.
The ADC16 output value is 215.
.............................
.............................