MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • TWR-KM35Z75M board

  • Personal Computer

Board settings#

This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.

Prepare the Demo#

  1. Connect a USB cable between the PC host and the OpenSDA USB port on the board.

  2. Download the program to the target board.

  3. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

When the demo runs successfully, you will find the LED is blinking.