Hardware requirements#
Micro USB cable
TWR-KM35Z75M board
Personal Computer
Board settings#
Connect J21 1-2 to use potentiometer
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
Roll the potentiometer(R21) to change the ADC value. When the demo runs successfully, the following message is displayed in the terminal:
ADC16 polling Example.
ADC16_DoAutoCalibration() Done.
Press any key to get user channel's ADC value ...
ADC Value: 1985
ADC Value: 1689
ADC Value: 1355
ADC Value: 1625
ADC Value: 1575
ADC Value: 1471