Hardware requirements
Micro USB cable
TWR-KM35Z75M board
Personal Computer
Elevator Tower
Board settings
No special setting are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Connect the analog signal source’s output to the input of used-defined comparator’s channel (defined as “DEMO_CMP_USER_CHANNEL” in source code.)
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the following message is displayed in the terminal:
CMP polling Example
Then change CMP analog input, and watch the change of LED. - CMP0_IN1 (Jump A63 on Elevator Tower) connected to VCC=3.3V (Jump B3 on Elevator Tower): LED ORANGE on - CMP0_IN1 (Jump A63 on Elevator Tower) connected to GND ( Jump B2 on Elevator Tower): LED ORANGE off