Hardware requirements

  • J-Link ARM

  • TWR-KM35Z75M board

  • Micro USB cable

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:

Press anykey to start the example...

EWM example
Press SW1 to expire EWM
EWM interrupt is occurred
Press SW1 to expire EWM again