MCUXpresso SDK Documentation

ZPS_eAplZdpMgmtDirectJoinRequest

ZPS_eAplZdpMgmtDirectJoinRequest#

ZPS_teStatus ZPS_eAplZdpMgmtDirectJoinRequest(
            PDUM_thAPduInstance hAPduInst,
            ZPS_tuAddress uDstAddr,
            bool bExtAddr,
            uint8 *pu8SeqNumber,
            ZPS_tsAplZdpMgmtDirectJoinReq
            *psZdpMgmtDirectJoinReq);

Description#

This function requests a remote node to allow a particular device (identified through its IEEE address) to join the network as a child of the node. Thus, joining should be enabled on the remote node just for the nominated device. The destination node of this request must be a Router or the Coordinator.

Note: This function is provided in the ZDP API for the reason of interoperability with nodes running non-NXP ZigBee PRO stacks that support the generated request. On receiving a request from this function, the NXP ZigBee PRO stack will return the status ZPS_ZDP_NOT_SUPPORTED.

The IEEE address of the nominated device as well as its capabilities must be included in the request. The request is represented by the structure below (further detailed in Section 8.2.2.38).

typedef struct {

uint64 u64DeviceAddress; uint8 u8Capability;

} ZPS_tsAplZdpMgmtDirectJoinReq;

The remote node replies with a Mgmt_Direct_Join_req response, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpMgmtDirectJoinRsp(detailed in Section 8.2.3.38).

Parent topic:ZPS_eAplZdpMgmtDirectJoinRequest

Parameters#

  • hAPduInst Handle of APDU instance in which request is sent.

  • uDstAddr Address of destination node of request (can be 16-bit or 64-bit, as specified by bExtAddr)

  • bExtAddr Type of destination address:

    • TRUE: 64-bit IEEE (MAC) address

    • FALSE: 16-bit network address

  • * pu8SeqNumber Pointer to sequence number of request

  • * psZdpMgmtDirectJoinReq Pointer to request (see above)

Parent topic:ZPS_eAplZdpMgmtDirectJoinRequest

Returns#

  • ZPS_E_SUCCESS (request successfully sent)

  • APS return codes, listed and described in Section 11.2.2

  • NWK return codes, listed and described in Section 11.2.3

  • MAC return codes, listed and described in Section 11.2.4

Parent topic:ZPS_eAplZdpMgmtLeaveRequest

Parent topic:ZPS_eAplZdpMgmtDirectJoinRequest

Parent topic:ZPS_eAplZdpMgmtPermitJoiningRequest

Parent topic:ZPS_eAplZdpMgmtCacheRequest

Parent topic:Network Management Services functions