MCUXpresso SDK Documentation

ZPS_eAplZdpMgmtPermitJoiningRequest

ZPS_eAplZdpMgmtPermitJoiningRequest#

ZPS_teStatus ZPS_eAplZdpMgmtPermitJoiningRequest(
            PDUM_thAPduInstance hAPduInst,
            ZPS_tuAddress uDstAddr,
            bool bExtAddr,
            uint8 *pu8SeqNumber,
            ZPS_tsAplZdpMgmtPermitJoiningReq
            *psZdpMgmtPermitJoiningReq);

Description#

This function requests a remote node to enable or disable joining for a specified amount of time. The destination node of this request must be a Router or the Co- ordinator. The request can be unicast to a particular node or broadcast to all routing nodes (for which the destination address must be set to the 16-bit network address 0xFFFC).

Note: This function is provided in the ZDP API for the reason of interoperability with nodes running non-NXP ZigBee PRO stacks that support the generated request. On receiving a request from this function, the NXP ZigBee PRO stack will return the status ZPS_ZDP_NOT_SUPPORTED.

The duration of the enable or disable joining state must be specified in the request. The request is represented by the structure below (further detailed in Section8.2.2.39).

typedef struct {

uint8 u8PermitDuration; bool_t bTcSignificance;

} ZPS_tsAplZdpMgmtPermitJoiningReq;

If the request was unicast, the remote node replies with a Mgmt_Permit_Joining_rsp response, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpMgmtPermitJoiningRsp(detailed in Section 8.2.3.39).

Parent topic:ZPS_eAplZdpMgmtPermitJoiningRequest

Parameters#

  • hAPduInst Handle of APDU instance in which request is sent.

  • uDstAddr Address of destination node of request (can be 16-bit or 64-bit, as specified by bExtAddr)

  • bExtAddr Type of destination address:

    • TRUE: 64-bit IEEE (MAC) address

    • FALSE: 16-bit network address

  • * pu8SeqNumber Pointer to sequence number of request

  • * psZdpMgmtPermitJoiningReqPointer to request (see above)

Parent topic:ZPS_eAplZdpMgmtPermitJoiningRequest

Returns#

  • ZPS_E_SUCCESS (request successfully sent)

  • APS return codes, listed and described in Section 11.2.2

  • NWK return codes, listed and described in Section 11.2.3

  • MAC return codes, listed and described in Section 11.2.4

Parent topic:ZPS_eAplZdpMgmtLeaveRequest

Parent topic:ZPS_eAplZdpMgmtDirectJoinRequest

Parent topic:ZPS_eAplZdpMgmtPermitJoiningRequest

Parent topic:ZPS_eAplZdpMgmtCacheRequest

Parent topic:Network Management Services functions