MCUXpresso SDK Documentation

ZPS_eAplZdpMgmtLeaveRequest

ZPS_eAplZdpMgmtLeaveRequest#

ZPS_teStatus ZPS_eAplZdpMgmtLeaveRequest(
            PDUM_thAPduInstance hAPduInst,
            ZPS_tuAddress uDstAddr,
            bool bExtAddr,
            uint8 *pu8SeqNumber,
            ZPS_tsAplZdpMgmtLeaveReq *psZdpMgmtLeaveReq);

Description#

This function requests a remote node to leave the network. The request also indicates whether the children of the leaving node should also be requested to leave and whether the leaving node(s) should subsequently attempt to rejoin the network.

Note: This function is provided in the ZDP API for the reason of interoperability with nodes running non-NXP ZigBee PRO stacks that support the generated request. On receiving a request from this function, the NXP ZigBee PRO stack will return the status ZPS_ZDP_NOT_SUPPORTED.

The IEEE address of the node to leave the network must be included in the request, as well as flags indicating the children and rejoin choices (see above). The request is represented by the structure below (further detailed in Section 8.2.2.37).

typedef struct {

uint64 u64DeviceAddress;

uint8 u8Flags;

} ZPS_tsAplZdpMgmtLeaveReq;

The remote node replies with a Mgmt_Leave_rsp response, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpMgmtLeaveRsp(detailed in Section 8.2.3.37).

Parent topic:ZPS_eAplZdpMgmtLeaveRequest

Parameters#

  • hAPduInst Handle of APDU instance in which request is sent.

  • uDstAddr Address of destination node of request (can be 16-bit or 64-bit, as specified by bExtAddr)

  • bExtAddr Type of destination address:

    • TRUE: 64-bit IEEE (MAC) address

    • FALSE: 16-bit network address

  • * pu8SeqNumber Pointer to sequence number of request

  • * psZdpMgmtLeaveReq Pointer to request (see above)

Parent topic:ZPS_eAplZdpMgmtLeaveRequest

Returns#

  • ZPS_E_SUCCESS (request successfully sent)

  • APS return codes, listed and described in Section 11.2.2

  • NWK return codes, listed and described in Section 11.2.3

  • MAC return codes, listed and described in Section 11.2.4

Parent topic:ZPS_eAplZdpMgmtLeaveRequest

Parent topic:ZPS_eAplZdpMgmtDirectJoinRequest

Parent topic:ZPS_eAplZdpMgmtPermitJoiningRequest

Parent topic:ZPS_eAplZdpMgmtCacheRequest

Parent topic:Network Management Services functions