MCUXpresso SDK Documentation

Hardware requirements#

  • Type-C USB cable

  • FRDM-IMXRT700

  • Personal Computer

  • RaspberryPi Panel

Board settings#

Connect JP1 and JP3.

To use Raspberry panel: Connect the panel to J8. Then connect the panel’s 5V pin to JP43-1, GND pin to JP43-2.

Project Configuration#

Refer the section Display Settings in file examples_share_readme.md.

Prepare the Demo#

The demo use MIPI Raspberry panel by default, to use other panel, see Steps to select the panel. The supported panels can be found in examples/_boards/frdmimxrt700/project_segments/display_support/Kconfig.prjseg. Or change the macro DEMO_PANEL in mcux_config.h of the project, which number represents which panel can be found in display_support.h and mcux_config.h

  1. Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

When the example runs, you can see the picture displayed in the up left corner of the panel.