MCUXpresso SDK Documentation

Scenes Cluster

Contents

Scenes Cluster#

This chapter describes the Scenes cluster that allows scenes to be managed.

The Scenes cluster has a Cluster ID of 0x0005.

Overview#

A scene is a set of stored attribute values for one or more cluster instances, where these cluster instances may exist on endpoints on one or more devices.

The Scenes cluster allows standard values for these attributes to be set and retrieved. Thus, the cluster can be used to put the network or part of the network into a pre-defined mode (for example, Night or Day mode for a lighting network). These pre-defined scenes can be used as a basis for ‘mood lighting’. A Scenes cluster instance must be created on each endpoint which contains a cluster that is part of a scene.

A scene is often associated with a group (which collects together a set of endpoints over one or more devices) - groups are described in Chapter 12. A scene may, however, be used without a group.

Note: When the Scenes cluster is used on an endpoint, a Groups cluster instance must always be created on the same endpoint, even if a group is not used for the scene.

If a cluster on a device is used in a scene, an entry for the scene must be contained in the Scene table on the device. A Scene table entry includes the scene ID, the group ID associated with the scene (0x0000 if there is no associated group), the scene transition time (amount of time to switch to the scene), and the attribute settings for the clusters on the device. The scene ID must be unique within the group with which the scene is associated.

To use the functionality of this cluster, you must include the file Scenes.h in your application and enable the cluster by defining CLD_SCENES in the zcl_options.h file.

It is also necessary to enable the cluster as a server or client, or as both:

  • The cluster server is able to receive commands to access scenes.

  • The cluster client is able to send commands to the server to request read or write access to scenes.

The inclusion of the client or server software must be pre-defined in the compile-time options of the application (in addition, if the cluster is to reside on a custom endpoint then the role of client or server must also be specified when creating the cluster instance).

The compile-time options for the Scenes cluster are fully detailed in Section 13.9.

Parent topic:Scenes Cluster

Scenes Cluster structure and attributes#

The structure definition for the Scenes cluster is:

typedef struct
{
#ifdef SCENES_SERVER
   zuint8  u8SceneCount;
   zuint8  u8CurrentScene;
   zuint16 u16CurrentGroup;
   zbool   bSceneValid;
   zuint8  u8NameSupport;
#ifdef CLD_SCENES_ATTR_LAST_CONFIGURED_BY
   zieeeaddress  u64LastConfiguredBy;
#endif
#endif
    zuint16 u16ClusterRevision;
} tsCLD_Scenes;

where:

  • u8SceneCount is the number of scenes currently in the Scene table.

  • u8CurrentScene is the scene ID of the last scene invoked on the device.

  • u16CurrentGroup is the group ID of the group associated with the last scene invoked (or 0x0000 if this scene is not associated with a group).

  • bSceneValid indicates whether the current state of the device corresponds to the values of the CurrentScene and CurrentGroup attributes (TRUE if they do, FALSE if they do not).

  • u8NameSupport indicates whether scene names are supported - if the most significant bit is 1 then they are supported, otherwise they are not supported.

  • u64LastConfiguredBy is the 64-bit IEEE address of the device that last configured the Scene table (0xFFFFFFFFFFFFFFFF indicates that the address is unknown or the table has not been configured).

  • u16ClusterRevision is a mandatory attribute that specifies the revision of the cluster specification on which this cluster instance is based. The cluster specification in the ZCL r6 corresponds to a cluster revision of 1. The value is incremented by one for each subsequent revision of the cluster specification. This attribute is also described in Section 2.4.

Parent topic:Scenes Cluster

Initialization#

The function eCLD_ScenesCreateScenes() is used to create an instance of the Scenes cluster. The function is generally called by the initialization function for the host device.

Parent topic:Scenes Cluster

Sending Remote Commands#

The NXP implementation of the ZCL provides functions for sending commands between a Scenes cluster client and server. A command is sent from the client to one or more endpoints on the server. Multiple endpoints can usually be targeted using binding or group addressing.

Note: Commands can also be issued for operations on the local node, as described in Section 13.5.

Creating a Scene#

In order to create a scene, add an entry for the scene to the Scene table on every device that contains a cluster, which is associated with the scene.

Use the function eCLD_ScenesCommandAddSceneRequestSend() to request a scene to be added to a Scene table on a remote device. Invoking this function sends a request to a single device or to multiple devices (using binding or group addressing). The fields of the Scene table entry are specified in the payload of the request.

Alternatively:

  • The function eCLD_ScenesCommandEnhancedAddSceneRequestSend() can be used to request that a scene is added to a Scene table on a remote device. This method allows the transition time for the scene to be set in units of tenths of a second (rather than seconds).

  • A scene can be created by saving the current attribute settings of the relevant clusters. In this way, the current state of the system can be captured as a scene and reapplied ‘at the touch of a button’ when required. For example scenes can be created for lighting levels in a ‘smart lighting’ system. The current settings are stored as a scene in the Scene table using eCLD_ScenesCommandStoreSceneRequestSend(). This function can send the request to a single device or multiple devices. If a Scene table entry exists with the same scene ID and group ID, the existing cluster settings in the entry are overwritten with the new ‘captured’ settings.

Note: This operation of capturing the current system state as a scene does not result in meaningful settings for the transition time and scene name fields of the Scene table entry. If non-null values are required for these fields, the table entry should be created in advance with the desired field values using eCLD_ScenesCommandAddSceneRequestSend().

Parent topic:Sending Remote Commands

Copying a Scene#

Scene settings can be copied from one scene to another scene on the same remote endpoint using the eCLD_ScenesCommandCopySceneSceneRequestSend() function. This function allows the settings from an existing scene with a specified source scene ID and associated group ID to be copied to a new scene with a specified destination scene ID and associated group ID.

Note: If an entry corresponding to the target scene ID and group ID exists in the Scene table on the endpoint, the entry settings are overwritten with the copied settings. Otherwise, a new Scene table entry is created with these settings.

The above function also allows all scenes associated with particular group ID to be copied to another group ID. In this case, the original scene IDs are maintained but are associated with the new group ID (any specified source and destination scene IDs are ignored). Thus, the same scene IDs are associated with two different group IDs.

Parent topic:Sending Remote Commands

Applying a Scene#

The cluster settings of a scene stored in the Scene table can be retrieved and applied to the system by calling eCLD_ScenesCommandRecallSceneRequestSend(). Again, this function can send a request to a single device or to multiple devices (using binding or group addressing).

If the required scene does not contain any settings for a particular cluster or there are some missing attribute values for a cluster, these attribute values remain unchanged in the implementation of the cluster - that is, the corresponding parts of the system do not change their states.

Parent topic:Sending Remote Commands

Deleting a Scene#

Two functions are provided for removing scenes from the system:

  • eCLD_ScenesCommandRemoveSceneRequestSend() can be used to request the removal of the destination endpoint from a particular scene - that is, to remove the scene from the Scene table on the target device.

  • eCLD_ScenesCommandRemoveAllScenesRequestSend() can be used to request that the target device removes scenes associated with a particular group ID/address - that is, remove all Scene table entries relating to this group ID. Specifying a group ID of 0x0000 removes all scenes not associated with a group.

Parent topic:Sending Remote Commands

Obtaining Information about Scenes#

The following functions are provided for obtaining information about scenes:

  • eCLD_ScenesCommandViewSceneRequestSend() can be used to request information on a particular scene on the destination endpoint. Only one device may be targeted by this function. The target device returns a response containing the relevant information.

    • Alternatively, eCLD_ScenesCommandEnhancedViewSceneRequestSend() can be used, which allows the transition time for the scene to be obtained in units of tenths of a second (rather than seconds).

  • eCLD_ScenesCommandGetSceneMembershipRequestSend() can be used to discover which scenes are associated with a particular group on a device. The request can be sent to a single device or to multiple devices. The target device returns a response containing the relevant information (in the case of multiple target devices, no response is returned from a device that does not contain a scene associated with the specified group ID). In this way, the function can be used to determine the unused scene IDs.

Parent topic:Sending Remote Commands

Parent topic:Scenes Cluster

Issuing Local Commands#

Some of the operations described in Section 13.4 that correspond to remote commands can also be performed locally, as described below.

Creating a Scene#

A scene can be created on the local node using either of the following functions:

  • eCLD_ScenesAdd(): This function can be used to add a new scene to the Scene table on the specified local endpoint. A scene ID and an associated group ID must be specified (the latter must be set to 0x0000 if there is no group association). If a scene with these IDs exists in the table, the existing entry is overwritten.

  • eCLD_ScenesStore(): This function can be used to save the currently implemented attribute values on the device to a scene in the Scene table on the specified local endpoint. A scene ID and an associated group ID must be specified (the latter must be set to 0x0000 if there is no group association). If a scene with these IDs exists in the table, the existing entry is overwritten except for the transition time and scene name fields.

Parent topic:Issuing Local Commands

Applying a Scene#

An existing scene can be applied on the local node using the function eCLD_ScenesRecall(). This function reads the stored attribute values for the specified scene from the local Scene table and implements them on the device. The values of any attributes that are not included in the scene remain unchanged.

Parent topic:Issuing Local Commands

Parent topic:Scenes Cluster

Functions#

The following Scenes cluster functions are provided in the NXP implementation of the ZCL:

  1. eCLD_ScenesCreateScenes

  2. eCLD_ScenesAdd

  3. eCLD_ScenesStore

  4. eCLD_ScenesRecall

  5. eCLD_ScenesCommandAddSceneRequestSend

  6. eCLD_ScenesCommandViewSceneRequestSend

  7. eCLD_ScenesCommandRemoveSceneRequestSend

  8. eCLD_ScenesCommandRemoveAllScenesRequestSend

  9. eCLD_ScenesCommandStoreSceneRequestSend

  10. eCLD_ScenesCommandRecallSceneRequestSend

  11. eCLD_ScenesCommandGetSceneMembershipRequestSend

  12. eCLD_ScenesCommandEnhancedAddSceneRequestSend

  13. eCLD_ScenesCommandEnhancedViewSceneRequestSend

  14. eCLD_ScenesCommandCopySceneSceneRequestSend

eCLD_ScenesCreateScenes#

teZCL_Status eCLD_ScenesCreateScenes(
    tsZCL_ClusterInstance *psClusterInstance,
    bool_t bIsServer,
    tsZCL_ClusterDefinition *psClusterDefinition,
    void *pvEndPointSharedStructPtr,
    uint8 *pu8AttributeControlBits,
    tsCLD_ScenesCustomDataStructure
    *psCustomDataStructure,
tsZCL_EndPointDefinition *psEndPointDefinition);

Description#

This function creates an instance of the Scenes cluster on an endpoint. The cluster instance is created on the endpoint which is associated with the supplied tsZCL_ClusterInstance structure and can act as a server or a client, as specified.

The function should be called when setting up a custom endpoint containing one or more selected clusters (rather than the whole set of clusters supported by a standard ZigBee device). This function creates a Scenes cluster instance on the endpoint, but instances of other clusters may also be created on the same endpoint by calling their corresponding creation functions.

Note: Do not call this function for an endpoint on which a standard ZigBee device is used. In this case, the device and its supported clusters must be registered on the endpoint using the relevant device registration function.

When used, this function must be the first Scenes cluster function called in the application, and must be called after the stack has been started and after the ZCL has been initialized.

On calling this function for the first time, a ‘global scene’ entry is created/reserved in the Scene table. On subsequent calls (for example, following a power-cycle or on waking from sleep), if the scene data is recovered by the application from non-volatile memory before the function is called then there is no reinitialization of the scene data. Note that removing all groups from the device also removes the global scene entry (along with other scene entries) from the Scene table.

The function requires an array to be declared for internal use, which contains one element (of type uint8) for each attribute of the cluster. The array length should therefore equate to the total number of attributes supported by the Scene cluster.

The function initializes the array elements to zero.

Parameters#

  • psClusterInstance: Pointer to structure containing information about the cluster instance to be created (see Section 6.1.16). This structure is updated by the function by initializing individual structure fields.

  • bIsServer: Type of cluster instance (server or client) to be created:

    • TRUE - server

    • FALSE - client

  • psClusterDefinition: Pointer to structure indicating the type of cluster to be created (see Section 6.1.2). In this case, this structure must contain the details of the Scenes cluster. This parameter can refer to a pre-filled structure called sCLD_Scenes which is provided in the Scenes.h file.

  • pvEndPointSharedStructPtr: Pointer to the shared structure used for attribute storage. This parameter should be the address of the structure of type tsCLD_Scenes which defines the attributes of Scenes cluster. The function initializes the attributes with default values.

  • pu8AttributeControlBits: Pointer to an array of uint8 values, with one element for each attribute in the cluster (see above).

  • psCustomDataStructure: Pointer to a structure containing the storage for internal functions of the cluster (see Section 13.7.1)

  • psEndPointDefinition: Pointer to the ZCL endpoint definition structure for the application (see Section 6.1.1)

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

Parent topic:Functions

eCLD_ScenesAdd#

teZCL_Status eCLD_ScenesAdd(
    uint8 u8SourceEndPointId,
    uint16 u16GroupId,
    uint8 u8SceneId);   

Description#

This function adds a new scene on the specified local endpoint - that is, adds an entry to the Scenes table on the endpoint. The group ID associated with the scene must also be specified (or set to 0x0000 if there is no associated group).

If a scene with the specified scene ID and group ID exists in the table, the existing entry is overwritten (that is, all previous scene data in this entry is lost).

Parameters#

  • u8SourceEndPointId: Number of local endpoint on which Scene table entry is to be added.

  • u16GroupId: 16-bit group ID/address of associated group (or 0x0000 if no group).

  • u8SceneId: 8-bit scene ID of new scene.

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

Parent topic:Functions

eCLD_ScenesStore#

teZCL_Status eCLD_ScenesStore(
    uint8 u8SourceEndPointId,
    uint16 u16GroupId,
    uint8 u8SceneId);

Description#

This function adds a new scene on the specified local endpoint, based on the current cluster attribute values of the device- that is, saves the current attribute values of the device to a new entry of the Scenes table on the endpoint. The group ID associated with the scene must also be specified (or set to 0x0000 if there is no associated group).

If a scene with the specified scene ID and group ID exists in the table, the existing entry is overwritten. The previous scene data in this entry is lost, except for the transition time field and the scene name field - these fields are left unchanged.

Parameters#

  • u8SourceEndPointId: Number of local endpoint on which Scene table entry is to be added.

  • *u16GroupId:*16-bit group ID/address of associated group (or 0x0000 if no group)

  • u8SceneId: 8-bit scene ID of scene

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

Parent topic:Functions

eCLD_ScenesRecall#

teZCL_Status eCLD_ScenesRecall(
    uint8 u8SourceEndPointId,
    uint16 u16GroupId,
    uint8 u8SceneId);

Description#

This function obtains the attribute values (from the extension fields) of the scene with the specified Scene ID and Group ID on the specified (local) endpoint, and sets the corresponding cluster attributes on the device to these values. Thus, the function reads the stored attribute values for a scene and implements them on the device.

Note that the values of any cluster attributes that are not included in the scene remains unchanged.

Parameters#

  • u8SourceEndPointId: Number of local endpoint containing Scene table to be read.

  • u16GroupId: 16-bit group ID/address of associated group (or 0x0000 if no group)

  • u8SceneId: 8-bit scene ID of scene to be read.

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

Parent topic:Functions

eCLD_ScenesCommandAddSceneRequestSend#

teZCL_Status eCLD_ScenesCommandAddSceneRequestSend(
    uint8 u8SourceEndPointId,
    uint8 u8DestinationEndPointId,
    tsZCL_Address *psDestinationAddress,
    uint8 *pu8TransactionSequenceNumber,
    tsCLD_ScenesAddSceneRequestPayload *psPayload);

Description#

This function sends an Add Scene command to a remote device in order to add a scene on the specified endpoint - that is, to add an entry to the Scene table on the endpoint. The scene ID is specified in the payload of the message, along with a duration for the scene among other values (see Section 13.7.2). The scene may also be associated with a particular group.

The device receiving this message generates a callback event on the endpoint on which the Scenes cluster is registered and, if possible, add the scene to its Scene table before sending an Add Scene response indicating success or failure (see Section 13.7.3).

You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

Parameters#

  • u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.

  • u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP.

  • psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.

  • pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.

    • psPayload: Pointer to a structure containing the payload for this message (see Section 13.7.2)

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_FAIL

If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().

Parent topic:Functions

eCLD_ScenesCommandViewSceneRequestSend#

teZCL_Status eCLD_ScenesCommandViewSceneRequestSend(
    uint8 u8SourceEndPointId,
    uint8 u8DestinationEndPointId,
    tsZCL_Address *psDestinationAddress,
    uint8 *pu8TransactionSequenceNumber,
    tsCLD_ScenesViewSceneRequestPayload
*psPayload);

Description#

This function sends a View Scene command to a remote device, requesting information on a particular scene on the destination endpoint. The relevant scene ID is specified in the command payload. Note that this command can only be sent to an individual device/endpoint and not to a group address.

The device receiving this message generates a callback event on the endpoint on which the Scenes cluster was registered and generates a View Scene response containing the relevant information (see Section 13.7.3).

You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

Parameters#

  • u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.

  • u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address type eZCL_AMBOUND.

  • psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.

  • pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.

  • psPayload: Pointer to a structure containing the payload for this message (see Section 13.7.2)

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_FAIL

If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().

Parent topic:Functions

eCLD_ScenesCommandRemoveSceneRequestSend#

teZCL_Status eCLD_ScenesCommandRemoveSceneRequestSend(
    uint8 u8SourceEndPointId,
    uint8 u8DestinationEndPointId,
    tsZCL_Address *psDestinationAddress,
    uint8 *pu8TransactionSequenceNumber,
    tsCLD_ScenesRemoveSceneRequestPayload
*psPayload);

Description#

This function sends a Remove Scene command to request that the target device deletes membership of the destination endpoint from a particular scene - that is, remove the scene from the Scene table. The relevant scene ID is specified in the payload of the message. The scene may also be associated with a particular group.

The device receiving this message generates a callback event on the endpoint on which the Scenes cluster was registered. The device then deletes the scene in the Scene table. If the request was sent to a single device (rather than to a group address), it then generates an appropriate Remove Scene response indicating success, or failure (see Section 13.7.3).

You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

Parameters#

  • u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.

  • u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP.

  • psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.

  • pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.

  • psPayload: Pointer to a structure containing the payload for this message (see Section 13.7.2).

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_FAIL

If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().

Parent topic:Functions

eCLD_ScenesCommandRemoveAllScenesRequestSend#

teZCL_Status eCLD_ScenesCommandRemoveAllScenesRequestSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_ScenesRemoveAllScenesRequestPayload

Description#

This function sends a Remove All Scenes command to request that the target device deletes all entries corresponding to the specified group ID/address in its Scene table. The relevant group ID is specified in the payload of the message. Note that specifying a group ID of 0x0000 removes all scenes not associated with a group.

The device receiving this message generates a callback event on the endpoint on which the Scenes cluster was registered. The device then deletes the scenes in the Scene table. If the request is sent to a single device (rather than to a group address), it then generates an appropriate Remove All Scenes response indicating success, or failure (see Section 13.7.3).

You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

Parameters#

  • u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.

  • u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP.

  • psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.

  • pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.

  • psPayload: Pointer to a structure containing the payload for this message (see Section 13.7.2).

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_FAIL

If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().

Parent topic:Functions

eCLD_ScenesCommandStoreSceneRequestSend#

teZCL_Status eCLD_ScenesCommandStoreSceneRequestSend(
    uint8 u8SourceEndPointId,
    uint8 u8DestinationEndPointId,
    tsZCL_Address *psDestinationAddress,
    uint8 *pu8TransactionSequenceNumber,
    tsCLD_ScenesStoreSceneRequestPayload
*psPayload);

Description#

This function sends a Store Scene command to request that the target device saves the current settings of all other clusters on the device as a scene - that is, adds a scene containing the current cluster settings to the Scene table. The entry is stored using the scene ID and group ID specified in the payload of the command. If an entry exists with these IDs, its existing cluster settings are overwritten with the new settings.

Note that this command does not set the transition time and scene name fields (or for a new entry, they are set to null values). If this command is to create a new scene that requires particular settings for these fields, Add Group command should be used. The scene entry must be created in advance using the Add Group command, and the fields transition time and scene name should be pre-configured.

The device receiving this message generates a callback event on the endpoint on which the Scenes cluster was registered. If the request is sent to a single device (rather than to a group address), it then generates an appropriate Store Scene response indicating success, or failure (see Section 13.7.3).

You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

Parameters#

  • u8SourceEndPointId: ID or number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.

  • u8DestinationEndPointId: ID or number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP.

  • psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.

  • pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.

  • psPayload: Pointer to a structure containing the payload for this message (see Section 13.7.2).

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_F

If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().

Parent topic:Functions

eCLD_ScenesCommandRecallSceneRequestSend#

teZCL_Status eCLD_ScenesCommandRecallSceneRequestSend(
    uint8 u8SourceEndPointId,
    uint8 u8DestinationEndPointId,
    tsZCL_Address *psDestinationAddress,
    uint8 *pu8TransactionSequenceNumber,
    tsCLD_ScenesRecallSceneRequestPayload
    *psPayload);

Description#

This function sends a Recall Scene command to request that the target device retrieves and implements the settings of the specified scene - that is, reads the scene settings from the Scene table and applies them to the other clusters on the device. The required scene ID and group ID are specified in the payload of the command.

Note that if the specified scene entry does not contain any settings for a particular cluster or there are some missing attribute values for a cluster, these attribute values remains unchanged in the implementation of the cluster.

The device receiving this message generates a callback event on the endpoint on which the Scenes cluster was registered. If the request is sent to a single device (rather than to a group address), it then generates an appropriate Recall Scene response indicating success, or failure (see Section 13.7.3).

You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

Parameters#

  • u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.

  • u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP.

  • psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.

  • pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.

  • psPayload: Pointer to a structure containing the payload for this message (see Section 13.7.2).

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_FAIL

If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().

Parent topic:Functions

eCLD_ScenesCommandGetSceneMembershipRequestSend#

teZCL_Status eCLD_ScenesCommandGetSceneMembershipRequestSend(
    uint8 u8SourceEndPointId,
    uint8 u8DestinationEndPointId,
    tsZCL_Address *psDestinationAddress,
    uint8 *pu8TransactionSequenceNumber,
    tsCLD_ScenesGetSceneMembershipRequestPayload
*psPayload);

Description#

This function sends a Get Scene Membership to inquire which scenes are associated with a specified group ID on a device. The relevant group ID is specified in the payload of the command.

The device receiving this message generates a callback event on the endpoint on which the Scenes cluster is registered. If the request is sent to a single device (rather than to a group address), it then generates an appropriate Get Scene Membership response indicating success or failure and, if successful, the response contains a list of the scene IDs associated with the given group ID (see Section 13.7.3). If the original command is sent to a group address, an individual device only responds if it has scenes associated with the group ID in the command payload (so it only responds if successful).

You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

Parameters#

  • u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.

  • u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP.

  • psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.

  • pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.

  • psPayload: Pointer to a structure containing the payload for this message (see Section 13.7.2).

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_FAIL

If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().

Parent topic:Functions

eCLD_ScenesCommandEnhancedAddSceneRequestSend#

teZCL_Status eCLD_ScenesCommandEnhancedAddSceneRequestSend(
    uint8 u8SourceEndPointId,
    uint8 u8DestinationEndPointId,
    tsZCL_Address *psDestinationAddress,
    uint8 *pu8TransactionSequenceNumber,
    tsCLD_ScenesEnhancedAddSceneRequestPayload
*psPayload);

Description#

This function sends an Enhanced Add Scene command to a remote device in order to add a scene on the specified endpoint - that is, to add an entry to the Scene table on the endpoint. The function allows a finer transition time (in tenths of a second rather than seconds) when applying the scene. The scene ID is specified in the payload of the message, along with a duration for the scene and the transition time, among other values (see Section 13.7.2). The scene may also be associated with a particular group.

The device receiving this message generates a callback event on the endpoint on which the Scenes cluster is registered. If possible, add the scene to its Scene table before sending an Enhanced Add Scene response indicating success or failure (see Section 13.7.3).

You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

Parameters#

  • u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.

  • u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP.

  • psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.

  • pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.

  • psPayload: Pointer to a structure containing the payload for this message (see Section 13.7.2).

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_FAIL

If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().

Parent topic:Functions

eCLD_ScenesCommandEnhancedViewSceneRequestSend#

teZCL_Status eCLD_ScenesCommandEnhancedViewSceneRequestSend(
    uint8 u8SourceEndPointId,
    uint8 u8DestinationEndPointId,
    tsZCL_Address *psDestinationAddress,
    uint8 *pu8TransactionSequenceNumber,
    tsCLD_ScenesEnhancedViewSceneRequestPayload
*psPayload);

Description#

This function sends an Enhanced View Scene command to a remote device, requesting information on a particular scene on the destination endpoint. The returned information includes the finer transition time configured with the function eCLD_ScenesCommandEnhancedAddSceneRequestSend(). The relevant scene ID is specified in the command payload. Note that this command can only be sent to an individual device/endpoint and not to a group address.

The device receiving this message generates a callback event on the endpoint on which the Scenes cluster was registered and generates an Enhanced View Scene response containing the relevant information (see Section 13.7.3).

You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

Parameters#

  • u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.

  • u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address type eZCL_AMBOUND.

  • psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.

  • pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.

  • psPayload: Pointer to a structure containing the payload for this message (see Section 13.7.2)

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_FAIL

If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().

Parent topic:Functions

eCLD_ScenesCommandCopySceneSceneRequestSend#

teZCL_Status eCLD_ScenesCommandCopySceneSceneRequestSend(
    uint8 u8SourceEndPointId,
    uint8 u8DestinationEndPointId,
    tsZCL_Address *psDestinationAddress,
    uint8 *pu8TransactionSequenceNumber,
    tsCLD_ScenesCopySceneRequestPayload *psPayload);

Description#

This function sends a Copy Scene command to a remote device, requesting that the scene settings from one scene ID/group ID combination are copied to another scene ID/group ID combination on the target endpoint. The relevant source and destination scene ID/group ID combinations are specified in the command payload.

Note that:

  • If the destination scene ID/group ID exists on the target endpoint, the existing scene is overwritten with the new settings.

  • The message payload contains a ‘copy all scenes’ bit. If the bit is set to ‘1’, it instructs the destination server to copy all scenes in the specified source group to scenes with the same scene IDs in the destination group. In this case, the source and destination scene IDs in the payload are ignored.

The device receiving this message generates a callback event on the endpoint on which the Scenes cluster was registered and, if the original request is unicast, generates a Copy Scene response (see Section 13.7.3).

You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

Parameters#

  • u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.

  • u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address type eZCL_AMBOUND.

  • psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.

  • pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.

  • psPayload: Pointer to a structure containing the payload for this message (see Section 13.7.2).

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_FAIL

If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().

Parent topic:Functions

Parent topic:Scenes Cluster

Structures#

Custom Data Structure#

The Scenes cluster requires extra storage space to be allocated to be used by internal functions. The structure definition for this storage is shown below:

typedef struct
{
    DLIST   lScenesAllocList;
    DLIST   lScenesDeAllocList;
    tsZCL_ReceiveEventAddress       sReceiveEventAddress;
    tsZCL_CallBackEvent             sCustomCallBackEvent;
    tsCLD_ScenesCallBackMessage     sCallBackMessage;
    tsCLD_ScenesTableEntry
           asScenesTableEntry[CLD_SCENES_MAX_NUMBER_OF_SCENES];
} tsCLD_ScenesCustomDataStructure;

The fields are for internal use and no knowledge of them is required.

Parent topic:Structures

Custom Command Payloads#

The following structures contain the payloads for the Scenes cluster custom commands.

Add Scene Request Payload#

typedef struct
{
    uint16                      u16GroupId;
    uint8                       u8SceneId;
    uint16                      u16TransitionTime;
    tsZCL_CharacterString       sSceneName;
    tsCLD_ScenesExtensionField  sExtensionField;
} tsCLD_ScenesAddSceneRequestPayload;

where:

  • u16GroupId is the group ID with which the scene is associated (0x0000 if there is no association with a group)

  • u8SceneId is the ID of the scene to be added to the Scene table (the Scene ID must be unique within the group associated with the scene)

  • u16TransitionTime is the amount of time, in seconds, that the device takes to switch to this scene

  • sSceneName is an optional character string (of up to 16 characters) representing the name of the scene

  • sExtensionField is a structure containing the attribute values of the clusters to which the scene relates

View Scene Request Payload#

typedef struct
{
    uint16                      u16GroupId;
    uint8                       u8SceneId;
} tsCLD_ScenesViewSceneRequestPayload;

where:

  • u16GroupId is the group ID with which the desired scene is associated

  • u8SceneId is the scene ID of the scene to be viewed

Remove Scene Request Payload#

typedef struct
{
    uint16                      u16GroupId;
    uint8                       u8SceneId;
} tsCLD_ScenesRemoveSceneRequestPayload;

where:

  • u16GroupId is the group ID with which the relevant scene is associated

  • u8SceneId is the scene ID of the scene to be deleted from the Scene table

Remove All Scenes Request Payload#

typedef struct
{
    uint16                      u16GroupId;
} tsCLD_ScenesRemoveAllScenesRequestPayload;

where u16GroupId is the group ID for which all scenes are to be deleted.

Store Scene Request Payload#

typedef struct
{
    uint16                      u16GroupId;
    uint8                       u8SceneId;
} tsCLD_ScenesStoreSceneRequestPayload;

where:

  • u16GroupId is the group ID with which the relevant scene is associated

  • u8SceneId is the scene ID of the scene in which the captured cluster settings are to be stored

Recall Scene Request Payload#

typedef struct
{
    uint16                      u16GroupId;
    uint8                       u8SceneId;
} tsCLD_ScenesRecallSceneRequestPayload;

where:

  • u16GroupId is the group ID with which the relevant scene is associated

  • u8SceneId is the scene ID of the scene from which cluster settings are to be retrieved and applied

Get Scene Membership Request Payload#

typedef struct
{
    uint16                      u16GroupId;
} tsCLD_ScenesGetSceneMembershipRequestPayload;

where u16GroupId is the group ID for which associated scenes are required.

Enhanced Add Scene Request Payload#

typedef struct
{
    uint16                      u16GroupId;
    uint8                       u8SceneId;
    uint16                      u16TransitionTime100ms;
    tsZCL_CharacterString       sSceneName;
    tsCLD_ScenesExtensionField  sExtensionField;
} tsCLD_ScenesEnhancedAddSceneRequestPayload;

where:

  • u16GroupId is the group ID with which the scene is associated (0x0000 if there is no association with a group)

  • u8SceneId is the ID of the scene to be added to the Scene table (the Scene ID must be unique within the group associated with the scene)

  • u16TransitionTime100ms is the amount of time, in tenths of a second, that the device takes to switch to this scene

  • sSceneName is an optional character string (of up to 16 characters) representing the name of the scene

  • sExtensionField is a structure containing the attribute values of the clusters to which the scene relates

View Scene Request Payload#

typedef struct
{
    uint16                      u16GroupId;
    uint8                       u8SceneId;
} tsCLD_ScenesEnhancedViewSceneRequestPayload;

where:

  • u16GroupId is the group ID with which the desired scene is associated

  • u8SceneId is the scene ID of the scene to be viewed

Copy Scene Request Payload#

typedef struct
{
    uint8       u8Mode;
    uint16      u16FromGroupId;
    uint8       u8FromSceneId;
    uint16      u16ToGroupId;
    uint8       u8ToSceneId;
} tsCLD_ScenesCopySceneRequestPayload;

where:

  • u8Mode is a bitmap indicating the required copying mode (only bit 0 is used):

    • If bit 0 is set to ‘1’, then ‘copy all scenes’ mode is used, in which all scenes associated with the source group are duplicated for the destination group (and the scene ID fields are ignored)

    • If bit 0 is set to ‘0’, then a single scene is copied

  • u16FromGroupId is the source group ID

  • u8FromSceneId is the source scene ID (ignored for ‘copy all scenes’ mode)

  • u16ToGroupId is the destination group ID

  • u8ToSceneId is the destination scene ID (ignored for ‘copy all scenes’ mode)

Parent topic:Structures

Custom Command Responses#

The Scenes cluster generates responses to certain custom commands. The responses which contain payloads are detailed below:

Add Scene Response Payload#

typedef struct
{
    zenum8                      eStatus;
    uint16                      u16GroupId;
    uint8                       u8SceneId;
} tsCLD_ScenesAddSceneResponsePayload;

where:

  • eStatus is the outcome of the Add Scene command (success or invalid)

  • u16GroupId is the group ID with which the added scene is associated

  • u8SceneId is the scene ID of the added scene

View Scene Response Payload#

typedef struct
{
    zenum8                      eStatus;
    uint16                      u16GroupId;
    uint8                       u8SceneId;
    uint16                      u16TransitionTime;
    tsZCL_CharacterString       sSceneName;
    tsCLD_ScenesExtensionField  sExtensionField;
} tsCLD_ScenesViewSceneResponsePayload;

where:

  • eStatus is the outcome of the View Scene command (success or invalid)

  • u16GroupId is the group ID with which the viewed scene is associated

  • u8SceneId is the scene ID of the viewed scene

  • u16TransitionTime is the amount of time, in seconds, that the device takes to switch to the viewed scene

  • sSceneName is an optional character string (of up to 16 characters) representing the name of the viewed scene

  • sExtensionField is a structure containing the attribute values of the clusters to which the viewed scene relates

Remove Scene Response Payload#

typedef struct
{
    zenum8                      eStatus;
    uint16                      u16GroupId;
    uint8                       u8SceneId;
} tsCLD_ScenesRemoveSceneResponsePayload;

where:

  • eStatus is the outcome of the Remove Scene command (success or invalid)

  • u16GroupId is the group ID with which the removed scene is associated

  • u8SceneId is the scene ID of the removed scene

Remove All Scenes Response Payload#

typedef struct
{
    zenum8                      eStatus;
    uint16                      u16GroupId;
} tsCLD_ScenesRemoveAllScenesResponsePayload;

where:

  • eStatus is the outcome of the Remove All Scenes command (success or invalid)

  • u16GroupId is the group ID with which the removed scenes are associated

Store Scene Response Payload#

typedef struct
{
    zenum8                      eStatus;
    uint16                      u16GroupId;
    uint8                       u8SceneId;
} tsCLD_ScenesStoreSceneResponsePayload;

where:

  • eStatus is the outcome of the Store Scene command (success or invalid)

  • u16GroupId is the group ID with which the stored scene is associated

  • u8SceneId is the scene ID of the stored scene

Get Scene Membership Response Payload#

typedef struct
{
    zenum8                      eStatus;
    uint8                       u8Capacity;
    uint16                      u16GroupId;
    uint8                       u8SceneCount;
    uint8                       *pu8SceneList;
} tsCLD_ScenesGetSceneMembershipResponsePayload;

where:

  • eStatus is the outcome of the Get Scene Membership command (success or invalid)

  • u8Capacity is the capacity of the Scene table of the device to receive more scenes - that is, the number of scenes that may be added (special values: 0xFE means that at least one more scene may be added, a higher value means that the remaining capacity of the table is unknown)

  • u16GroupId is the group ID to which the query relates

  • u8SceneCount is the number of scenes in the list of the next field

  • pu8SceneList is a pointer to the returned list of scenes from those queried that exist on the device, where each scene is represented by its scene ID

Enhanced Add Scene Response Payload#

typedef struct
{
    zenum8     eStatus;
    uint16     u16GroupId;
    uint8      u8SceneId;
} tsCLD_ScenesEnhancedAddSceneResponsePayload;

where:

  • eStatus is the outcome of the Enhanced Add Scene command (success or invalid)

  • u16GroupId is the group ID with which the added scene is associated

  • u8SceneId is the scene ID of the added scene

Enhanced View Scene Response Payload#

typedef struct
{
    zenum8                      eStatus;
    uint16                      u16GroupId;
    uint8                       u8SceneId;
    uint16                      u16TransitionTime;
    tsZCL_CharacterString       sSceneName;
    tsCLD_ScenesExtensionField  sExtensionField;
} tsCLD_ScenesEnhancedViewSceneResponsePayload;

where:

  • eStatus is the outcome of the Enhanced View Scene command (success or invalid)

  • u16GroupId is the group ID with which the viewed scene is associated

  • u8SceneId is the scene ID of the viewed scene

  • u16TransitionTime is the amount of time, in seconds, that the device takes to switch to the viewed scene

  • sSceneName is an optional character string (of up to 16 characters) representing the name of the viewed scene

  • sExtensionField is a structure containing the attribute values of the clusters to which the viewed scene relates

Copy Scene Response Payload#

typedef struct
{
    uint8       u8Status;
    uint16      u16FromGroupId;
    uint8       u8FromSceneId;
} tsCLD_ScenesCopySceneResponsePayload;

where:

  • u8Status is the outcome of the Copy Scene command (success, invalid scene, or insufficient space for new scene)

  • u16FromGroupId is the source group ID for the copy

  • u8FromSceneId is the source scene ID for the copy

Parent topic:Structures

Scenes Table Entry#

The following structure contains the data for a Scenes table entry (containing a saved scene):

typedef struct
{
    DNODE          dllScenesNode;
    bool           bActive;
    bool           bInTransit;
    uint16         u16GroupId;
    uint8          u8SceneId;
    uint16         u16TransitionTime;
    uint32         u32TransitionTimer;
    uint8          u8SceneNameLength;
    uint8          au8SceneName[CLD_SCENES_MAX_SCENE_NAME_LENGTH + 1];
    uint16         u16SceneDataLength;
    uint8          au8SceneData[CLD_SCENES_MAX_SCENE_STORAGE_BYTES];
#ifdef  CLD_SCENES_TABLE_SUPPORT_TRANSITION_TIME_IN_MS
    uint8          u8TransitionTime100ms;
#endif
} tsCLD_ScenesTableEntry;

where:

  • bActive is a boolean value indicating whether the scene is active (TRUE) or inactive (FALSE).

  • bInTransit is a boolean value indicating whether the scene is in a transitional state (TRUE) or a constant active/inactive state (FALSE).

  • u16GroupId is the identifier of the group to which the scene applies (the value 0x0000 is used to indicate that the scene is not associated with a group).

  • u8SceneId is the identifier of the scene and must be a unique value within the group with which the scene is associated.

  • u16TransitionTime is the length of time, in seconds, that the device takes to move from its current state to the scene state.

  • u32TransitionTimer is the elapsed time, in milliseconds, since the start of a currently active transition to the scene.

  • u8SceneNameLength is the number of characters in the name of the scene (and therefore the size of the array au8SceneName[] below). The value must not be greater than CLD_SCENES_MAX_SCENE_NAME_LENGTH, which is set in the compile-time options (see Section 13.9).

  • au8SceneName[] is an array containing the name of the scene, with one ASCII character in each array element. The number of elements in the array must be set in u8SceneNameLength above.

  • u16SceneDataLength is the number of items of data for the scene (and therefore the size of the array au8SceneData[] below). The value must not be greater than CLD_SCENES_MAX_SCENE_STORAGE_BYTES, which is set in the compile-time options (see Section 13.9).

  • au8SceneData[] is an array containing the data for the scene, with one data item in each array element. The data stored is dependent on the cluster to which the scene data applies. The number of elements in the array must be set in u16SceneDataLength above.

  • u8TransitionTime 100 ms is an optional that allows a fractional part to be added to the transition time (u16TransitionTime) of the scene. This value represents the number of tenths of a second in the range 0x00 to 0x09.

Parent topic:Structures

Parent topic:Scenes Cluster

Enumerations#

teCLD_Scenes_ClusterID#

The following structure contains the enumerations used to identify the attributes of the Scenes cluster.

typedef enum 
{
    E_CLD_SCENES_ATTR_ID_SCENE_COUNT            = 0x0000,   /* Mandatory */
    E_CLD_SCENES_ATTR_ID_CURRENT_SCENE,                     /* Mandatory */
    E_CLD_SCENES_ATTR_ID_CURRENT_GROUP,                     /* Mandatory */
    E_CLD_SCENES_ATTR_ID_SCENE_VALID,                       /* Mandatory */
    E_CLD_SCENES_ATTR_ID_NAME_SUPPORT,                      /* Mandatory */
    E_CLD_SCENES_ATTR_ID_LAST_CONFIGURED_BY                 /* Optional  */
} teCLD_Scenes_ClusterID;

Parent topic:Enumerations

Parent topic:Scenes Cluster

Compile-time options#

To enable the Scenes cluster in the code to be built, it is necessary to add the following to the zcl_options.h file:

#define CLD_SCENES

In addition, to include the software for a cluster client or server or both, it is necessary to add one or both of the following to the same file:

#define SCENES_CLIENT
#define SCENES_SERVER

The Scenes cluster contains macros that may be optionally specified at compile time by adding some or all the following lines to the zcl_options.h file.

To enable the optional Last Configured By attribute, add this line:

#define CLD_SCENES_ATTR_LAST_CONFIGURED_BY

To configure the maximum length of the Scene Name storage, add this line:

#define CLD_SCENES_MAX_SCENE_NAME_LENGTH            (16)

To configure the maximum number of scenes, add this line:

#define CLD_SCENES_MAX_NUMBER_OF_SCENES             (16)

To configure the maximum number of bytes available for scene storage, add this line:

#define CLD_SCENES_MAX_SCENE_STORAGE_BYTES          (20)

To enable the Enhanced Add Scene command, add this line:

#define CLD_SCENES_CMD_ENHANCED_ADD_SCENE

To enable the Enhanced View Scene command, add this line:

#define CLD_SCENES_CMD_ENHANCED_VIEW_SCENE

To enable the Copy Scene command, add this line:

#define CLD_SCENES_CMD_COPY_SCENE

To enable TransitionTime100ms in Scene tables, add this line:

#define CLD_SCENES_TABLE_SUPPORT_TRANSITION_TIME_IN_MS

To define the value (n) of the Cluster Revision attribute, add this line:

#define CLD_SCENES_CLUSTER_REVISION <n>

The default value is 1, which corresponds to the revision of the cluster in the ZCL r6 specification (see Section 2.4).

Parent topic:Scenes Cluster