MCUXpresso SDK Documentation

Hardware requirements#

  • Mini/micro USB cable

  • EVK-MIMXRT1020 board

  • Personal Computer

Board settings#

No special settings are required.

Prepare the Demo#

  1. Connect a USB cable between the PC host and the OpenSDA USB on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo#

Consider special errata 005829 feature, the 1st valid MB should be used as reserved one. The TX MB number will change from 8 to 9, while RX MB number will change from 9 to 10 When the example runs successfully, following information can be seen on the OpenSDA terminal:


==FlexCAN loopback functional example -- Start.==


Send message from MB9 to MB10

tx word0 = 0x11223344

tx word1 = 0x55667788


Receved message from MB10

rx word0 = 0x11223344

rx word1 = 0x55667788


==FlexCAN loopback functional example -- Finish.==

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.