Hardware requirements#
Mini/micro USB cable
EVK-MIMXRT1064 board
Personal Computer
Board settings#
Connect input signal to J22-8.
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the example runs successfully, following information can be seen on the terminal:
GPT input capture example
Once the input signal is received the input capture value is printed