MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • FRDM-IMX95 board

  • JLink Plus

  • 12V~20V power supply

  • Personal Computer

Board settings#

No special is needed.

Prepare the Demo#

  1. Connect 12V~20V power supply and JLink Plus to the board, switch SW4 to power on the board

  2. Connect a micro USB cable between the host PC and the J31 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either re-power up your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

When the example runs successfully, following information can be seen on the terminal:


==FlexCAN loopback functional example -- Start.==


Send message from MB8 to MB9

tx word0 = 0x11223344

tx word1 = 0x55667788


Receved message from MB9

rx word0 = 0x11223344

rx word1 = 0x55667788


==FlexCAN loopback functional example -- Finish.==