Hardware requirements#
Type-C USB cable
FRDM-MCXA153 board
Personal Computer
Board settings#
Pin Name Board Location Pin Name Board Location
VREFI/P2_7 J3-1 VDD JP8-2
CMP0_IN0/P2_2 J2-9 VDD or GND
This example project uses LPCMP0 to compare the voltage signal input from CMP0_IN0(P2_2, J2-9) with the voltage signal(half of VREFI) output by LPCMP’s internal DAC. Connect J3-1(P2_7,VREFI) to JP8-2(VDD), this will set the VREFI to VDD(The VREFI is used as LPCMP reference voltage). Change the IO state of J2-9(P2_2, CMP0_IN0) will toggle the RED LED.
Prepare the Demo#
Connect a Type-C USB cable between the host PC and the MCU-Link port(J15) on the target board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The following lines are printed to the serial terminal when the demo program is executed.
LPCMP Polling Example.