Hardware requirements
- Micro USB cable 
- IMX95LP4X-EVK board 
- J-Link Debug Probe 
- 12V~20V power supply 
- Personal Computer 
Board settings
No special settings are required.
Please note this application can’t support running with Linux BSP!
Prepare the Demo
- Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board. 
- Connect a micro USB cable between the host PC and the J31 USB port on the target board. 
- Open a serial terminal with the following settings: - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board. 
- Either re-power up your board or launch the debugger in your IDE to begin running the example. 
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
Lpuart functional API interrupt example
Board receives characters then sends them out
Now please input: