MCUXpresso SDK Documentation

Arm GCC

Arm GCC#

  1. Navigate to <rt1064_install_dir>/boards/evkmimxrt1064/edgefast_bluetooth_examples/peripheral_ht/armgcc/.

  2. Copy folder from <rt1060evkc_install_dir>/boards/evkcmimxrt1060/edgefast_bluetooth_examples/template/ to <rt1064_install_dir>/boards/evkmimxrt1064/edgefast_bluetooth_examples/ and rename the files.

    |Path|Previous name|New name| |<rt1064_install_dir>/boards/evkmimxrt1064/edgefast_bluetooth_examples/|middleware_edgefast_bluetooth_mcux_linker_template_evkcmimxrt1060.cmake|middleware_edgefast_bluetooth_mcux_linker_template_evkmimxrt1064.cmake| |middleware_edgefast_bluetooth_sdio_template_evkcmimxrt1060.cmake|middleware_edgefast_bluetooth_sdio_template_evkmimxrt1064.cmake|

  3. Add the following content to<rt1064_install_dir>/devices/MIMXRT1064/all_lib_device.cmake at appropriate location.

    …
      ${CMAKE_CURRENT_LIST_DIR}/../../boards
      ${CMAKE_CURRENT_LIST_DIR}/../../boards/evkmimxrt1064/edgefast_bluetooth_examples/template
      ${CMAKE_CURRENT_LIST_DIR}/../../middleware/edgefast_bluetooth
      ${CMAKE_CURRENT_LIST_DIR}/../../middleware/wireless/ethermind
    …
    include_if_use(middleware_edgefast_bluetooth_ble_ethermind_cm7f)
    include_if_use(middleware_edgefast_bluetooth_ble_ethermind_lib_cm7f)
    include_if_use(middleware_edgefast_bluetooth_br_ethermind_cm7f)
    include_if_use(middleware_edgefast_bluetooth_br_ethermind_lib_cm7f)
    include_if_use(middleware_edgefast_bluetooth_btble_ethermind_cm7f)
    include_if_use(middleware_edgefast_bluetooth_btble_ethermind_lib_cm7f)
    include_if_use(middleware_edgefast_bluetooth_common_ethermind)
    include_if_use(middleware_edgefast_bluetooth_common_ethermind_hci)
    include_if_use(middleware_edgefast_bluetooth_common_ethermind_hci_uart)
    include_if_use(middleware_edgefast_bluetooth_config_ethermind)
    include_if_use(middleware_edgefast_bluetooth_config_template)
    include_if_use(middleware_edgefast_bluetooth_extension_common_ethermind)
    include_if_use(middleware_edgefast_bluetooth_k32w061_controller)
    include_if_use(middleware_edgefast_bluetooth_mcux_linker_template_ evkmimxrt1064)
    include_if_use(middleware_edgefast_bluetooth_pal)
    include_if_use(middleware_edgefast_bluetooth_pal_db_gen_ethermind)
    include_if_use(middleware_edgefast_bluetooth_pal_host_msd_fatfs_ethermind)
    include_if_use(middleware_edgefast_bluetooth_pal_platform_ethermind)
    include_if_use(middleware_edgefast_bluetooth_porting)
    include_if_use(middleware_edgefast_bluetooth_porting_atomic)
    include_if_use(middleware_edgefast_bluetooth_porting_list)
    include_if_use(middleware_edgefast_bluetooth_porting_net)
    include_if_use(middleware_edgefast_bluetooth_porting_toolchain)
    include_if_use(middleware_edgefast_bluetooth_porting_work_queue)
    include_if_use(middleware_edgefast_bluetooth_profile_bas)
    include_if_use(middleware_edgefast_bluetooth_profile_dis)
    include_if_use(middleware_edgefast_bluetooth_profile_fmp)
    include_if_use(middleware_edgefast_bluetooth_profile_hps)
    include_if_use(middleware_edgefast_bluetooth_profile_hrs)
    include_if_use(middleware_edgefast_bluetooth_profile_hts)
    include_if_use(middleware_edgefast_bluetooth_profile_ipsp)
    include_if_use(middleware_edgefast_bluetooth_profile_pxr)
    include_if_use(middleware_edgefast_bluetooth_profile_tip)
    include_if_use(middleware_edgefast_bluetooth_profile_wu)
    include_if_use(middleware_edgefast_bluetooth_sdio_template_evkmimxrt1064)
    include_if_use(middleware_edgefast_bluetooth_shell)
    include_if_use(middleware_edgefast_bluetooth_shell_ble)
    include_if_use(middleware_edgefast_bluetooth_template)
    include_if_use(middleware_edgefast_bluetooth_wifi_nxp_controller_base)...  
    
  4. Make the following changes in the listed order.

    File name

    Previous item

    New item

    config.cmake

    MIMXRT1062xxxxB

    MIMXRT1064xxxxA

    mflash_evkcmimxrt1060

    mflash_rt1064

    1062

    1064

    evkcmimxrt1060

    evkmimxrt1064

    flags.cmake

    1062

    1064

    6B

    6A

    CMakeLists.txt

    1062

    1064

    <rt1064_install_dir>/middleware/edgefast_bluetooth/middleware_edgefast_bluetooth_template.cmake

    evkcmimxrt1060

    evkmimxrt1064

    <rt1064_install_dir>/middleware/wireless/ethermind/middleware_edgefast_bluetooth_common_ethermind_hci_uart.cmake

    1062

    1064

    <rt1064_install_dir>/middleware/wireless/ethermind/ middleware_edgefast_bluetooth_k32w061_controller.cmake

    1062

    1064

    <rt1064_install_dir>/middleware/wireless/ethermind/middleware_edgefast_bluetooth_wifi_nxp_controller_base.cmake

    evkcmimxrt1060

    evkmimxrt1064

    <rt1064_install_dir>/boards/evkmimxrt1064/edgefast_bluetooth_examples/middleware_edgefast_bluetooth_mcux_linker_template_evkmimxrt1064.cmake

    1062

    1064

    <rt1064_install_dir>/boards/evkmimxrt1064/edgefast_bluetooth_examples/middleware_edgefast_bluetooth_sdio_template_evkmimxrt1064.cmake

    1062

    1064

  5. Rename MIMXRT1062xxxxx_flexspi_nor.ld as MIMXRT1064xxxxx_flexspi_nor.ld and make the following changes.

Parent topic:Migrate examples from RT1060EVKC to RT1064