Features

This section provides an overview of Bluetooth features, toolchain support, and RTOS support.

Bluetooth features

  • Bluetooth 5.0 compliant

  • Protocol support

    • L2CAP, GAP, GATT, RFCOMM, SDP, and SM

      Note: The Enhanced Attribute (EATT) protocol is not supported in the current version. However, the support will be available in a future version.

  • Classic profile

    • SPP, A2DP, and HFP

  • LE profile

    • HTP, PXP, IPSP, HPS

  • Integrated the Fatfs based on USB Host MSD in SDK

  • Digital Audio Interface including PCM interface for HFP

Parent topic:Features

Toolchain support

  • IAR Embedded Workbench for ARM®

  • MCUXpresso IDE

  • Keil® MDK/μVision

  • Makefiles support with GCC from Arm Embedded

Note: For details on IDE Development tools version details, see Section 3, Development tools in MCUXpresso SDK Release Notes (document MCUXSDKMIMXRT106XRN). The Release Notes document is available at root/docs/ MCUXpresso SDK Release Notes for EVK-MIMXRT1060.pdf.

Parent topic:Features

RTOS support

  • FreeRTOSTMOS

Parent topic:Features

Parent topic:Overview