MCUXpresso SDK Documentation

Contributing to the MCUboot project#

When contributing to MCUboot, please first discuss the changes you wish to make via issue, email or Discord.

Pull Request Process#

  1. Please ensure that the simulator tests pass. If you are modifying existing functionality, it may be sufficient to just ensure that these tests pass. If you are adding new functionality, you must also extend the simulator to test this new functionality.

  2. Ensure your changes follow the coding and style conventions for the files you are modifying (see below).

  3. If you wish (or are required to), be sure that copyright statements are up to date. Note that we follow the general guidance used in the Linux kernel, and adding a copyright statement is generally only acceptable for “significant” changes to a file.

  4. Be sure that all of your commits are signed off. Contributions must be released under the Apache 2.0 license, following the Developer Certificate of Origin.

  5. All contributions should follow the project code of conduct found in the root of the project directory.

  6. Pull requests will trigger various builds and tests. These must all pass.

  7. Non-trivial changes must have a release-note stub (see below).

Coding style and guidelines#

Mynewt coding#

A majority of the code in this project is written in C, and intended to run on embedded devices. This code began as a part of the mynewt RTOS, and still follows most of the coding conventions of that project. The primary exception is the copyright header, which is not appropriate as this is not an Apache project.

For files that came from MyNewt, we keep the existing Apache header, and add an additional header for MCUboot. In general, the following is sufficient.

/*
 * SPDX-License-Identifier: Apache-2.0
 */

this can be followed by individual contributor copyrights, if that is necessary.

General guidelines#

Although MCUboot needs to be small and compact, please try to hold back on the use of ifdefs in the code. It is better to factor out common code, and have different features in separate files, protected by a single ifdef than to have a large function with ifdefs sprinkled throughout it.

Simulator coding#

The simulator sim is an important part of what makes mcuboot reliable and robust. As such, it is important to make sure that changes made to the code are being tested by the simulator.

The simulator puts the boot code through an intense stress test, testing thousands of possibly failures (including numerous power failure conditions). It would take very long, and be very difficult to test these cases on target, and most devices would wear out after just a few runs.

As such, development should primarily be done using the simulator. Testing on actual targets should be done after the code is working in the simulator, as a sanity test that it really works.

Because of this, changes that change the behavior of the bootloader need to also be demonstrated to be tested by the simulator. For many changes, this means changing the simulator itself to test the new configuration. For example, a change that makes a new device work needs to have that device’s flash configuration added to the simulator to demonstrate that it doesn’t cause problems with corner cases and bad powerdowns.

Running the simulator#

CI will run the simulator through a multitude of configurations. See .github/workflows/sim.yaml for a full list. Individual configurations can easily be tested from the command line with something like:

$ cargo test \
    --features "sig-ecdsa-mbedtls swap-move" \
    -- --nocapture --test-threads 1

Additional arguments will be patterns to match the tests cases that can be run.

To run one of these tests in the debugger, you can do something like:

$ cargo test --features "swap-move" --no-run

This will print out the executables generated, and you will typically want the executable that starts with ‘core-’ followed by a hash.

Running this executable, with the --nocapture --test-threads 1 arguments, and possibly test filters can be done with the debugger to allow the debugger to be used on the code.

Release notes#

To facility creating release notes at release time, all non-trivial changes must include a release note snippet with the pull request. This can be either a separate commit, or as part of a single commit (generally, if there are multiple commits to the pull request, the release note snippet should be a separate commit, and a pull request that is a single commit can include the release note snippet in that commit).

The release notes should be placed in the docs/release-notes.d directory. Please see the readme file in that directory for specifics.