AF structures#
This section describes the structures of the Application Framework (AF) API. These include the following categories of structure:
Descriptor structures - see Section 8.2.1
Event structures - see Section 8.2.2
Other structures - see Section 8.2.3
Descriptor structures#
These structures are used to represent the following descriptors that contain information about the host node:
Node descriptor
Node Power descriptor
Simple descriptor
The structures are listed below.
ZPS_tsAplAfNodeDescriptor#
The AF Node descriptor structure ZPS_tsAplAfNodeDescriptoris shown below.
typedef struct {
uint32 : 8;/* padding */
uint32 eLogicalType : 3;
uint32 bComplexDescAvail : 1;
uint32 bUserDescAvail : 1;
uint32 eReserved : 3; /* reserved */
uint32 eFrequencyBand : 5;
uint32 eApsFlags : 3;
uint32 u8MacFlags : 8;
uint16 u16ManufacturerCode;
uint8 u8MaxBufferSize;
uint16 u16MaxRxSize;
uint16 u16ServerMask;
uint16 u16MaxTxSize;
uint8 u8DescriptorCapability;
} ZPS_tsAplAfNodeDescriptor;
where:
eLogicalTypecontains 3 bits (bits 0-2) indicating the ZigBee device type of the node, as follows:000: Coordinator
001: Router
010: End Device
bComplexDescAvailis set to 1 if there is a Complex descriptor available for node.bUserDescAvailis set to 1 if there is a User descriptor available for node.eReservedis reserved.eFrequencyBandcontains 5 bits detailing the frequency bands supported by the node, as follows (a bit is set to 1 if the corresponding band is supported):Bit 0: 868-868.6 MHz
Bit 2: 902-928 MHz
Bit 3: 2400-2483.5 MHz
Bits 1 and 4 are reserved
eApsFlagsis not currently supported and set to zero.eMacFlagscontains 8 bits (bits 0-7) indicating the node capabilities, as required by the IEEE 802.15.4 MAC sub-layer. These node capability flags are described in the table: Table.u16ManufacturerCodecontains 16 bits (bits 0-15) indicating the manufacturer code for the node, where this code is allocated to the manufacturer by the ZigBee Alliance.u8MaxBufferSizeis the maximum size, in bytes, of an NPDU (Network Protocol Data Unit).u16MaxRxSizeis the maximum size, in bytes, of an APDU (Application Protocol Data Unit). This value can be greater than the value ofu8MaxBufferSize, due to the fragmentation of an APDU into NPDUs.u16ServerMaskcontains 8 bits (bits 0-7) indicating the server status of the node. This server mask is detailed in the table: Table.u16MaxTxSizeis the maximum size, in bytes, of the ASDU (Application Sub-layer Data Unit) in which a message can be sent (the message may actually be transmitted in smaller fragments)u8DescriptorCapabilitycontains 8 bits (bits 0-7) indicating the properties of the node that can be used by other nodes in network discovery, as follows:
Bit description of u8DescriptorCapability
Bit |
Description |
|---|---|
0 |
Set to 1 if Extended Active Endpoint List is available on the node, 0 otherwise. |
1 |
Set to 1 if Extended Simple Descriptor List is available on the node, 0 otherwise. |
2-7 |
Reserved |
Parent topic:Descriptor structures
ZPS_tsAplAfNodePowerDescriptor#
The AF Node Power descriptor structure ZPS_tsAplAfNodePowerDescriptoris shown below.
typedef struct {
uint32 eCurrentPowerMode : 4;
uint32 eAvailablePowerSources : 4;
uint32 eCurrentPowerSource : 4;
uint32 eCurrentPowerSourceLevel : 4;
} ZPS_tsAplAfNodePowerDescriptor;
where:
eCurrentPowerModecontains 4 bits (bits 0-3) indicating the power mode currently used by the node, as follows:0000: Receiver configured according to “Receiver on when idle” MAC flag in the Node Descriptor (see Section 8.2.1.1)
0001: Receiver switched on periodically
0010: Receiver switched on when stimulated, for example, by pressing a button
All other values are reserved
eAvailablePowerSourcescontains 4 bits (bits 0-3) indicating the available power sources for the node, as follows (a bit is set to 1 if the corresponding power source is available):Bit 0: Permanent mains supply
Bit 1: Rechargeable battery
Bit 2: Disposable battery
Bit 4: Reserved
eCurrentPowerSourcecontains 4 bits (bits 0-3) indicating the current power source for the node, as detailed for the element above (the bit corresponding to the current power source is set to 1, all other bits are set to 0).eCurrentPowerSourceLevelcontains 4 bits (bit 0-3) indicating the current level of charge of the node’s power source (mainly useful for batteries), as follows:0000: Critically low
0100: Approximately 33%
1000: Approximately 66%
1100: Approximately 100% (near fully charged)
Parent topic:Descriptor structures
ZPS_tsAplAfSimpleDescriptor#
The AF Simple descriptor structure ZPS_tsAplAfSimpleDescriptoris shown below.
typedef struct {
uint16 u16ApplicationProfileId;
uint16 u16DeviceId;
uint8 u8DeviceVersion;
uint8 u8Endpoint;
uint8 u8InClusterCount;
uint8 u8OutClusterCount;
uint16 *pu16InClusterList;
uint16 *pu16OutClusterList;
} ZPS_tsAplAfSimpleDescriptor;
where:
u16ApplicationProfileIdis the 16-bit identifier of the ZigBee application profile supported by the endpoint. This must be an application profile identifier issued by the ZigBee Alliance (for Lighting and Occupancy devices, it is 0x0104).u16DeviceIdis the 16-bit identifier of the ZigBee device type supported by the endpoint. This must be a device type identifier issued by the ZigBee Alliance.u8DeviceVersioncontains 4 bits (bits 0-3) representing the version of the supported device description (default is 0000, unless set to another value according to the application profile used).u8Endpointis the number, in the range 1-240, of the endpoint to which the Simple descriptor corresponds.u8InClusterCountis an 8-bit count of the number of input clusters, supported on the endpoint, that will appear in the list pointed to by thepu16InClusterListelement.u8OutClusterCountis an 8-bit count of the number of output clusters, supported on the endpoint, that will appear in thepu16OutClusterListelement.*pu16InClusterListis a pointer to the list of input clusters supported by the endpoint (for use during the service discovery and binding procedures). This is a sequence of 16-bit values, representing the cluster numbers (in the range 1-240), where the number of values is equal to countu8InClusterCount. If this count is zero, the pointer can be set to NULL.*pu16OutClusterListis a pointer to the list of output clusters supported by the endpoint (for use during the service discovery and binding procedures). This is a sequence of 16-bit values, representing the cluster numbers (in the range 1-240), where the number of values is equal to countu8OutClusterCount. If this count is zero, the pointer can be set to NULL.
Parent topic:Descriptor structures
Parent topic:AF structures
Event structures#
These structures are used to contain events. Event details (type and associated data) are passed to the application in the structure ZPS_tsAfEvent. Data structures for the individual event types are contained in the union ZPS_tuAfEventData.
Enumerations for the event types are provided in the structure ZPS_teAfEventType. This structure and the associated events are detailed in Chapter 11, Event and Status Codes.
The structures are listed below.
ZPS_tsAfEvent#
This structure contains the details of an event. The ZPS_tsAfEventstructure is detailed below.
typedef struct {
ZPS_teAfEventType eType;
ZPS_tuAfEventData uEvent;
} ZPS_tsAfEvent;
where
eTypeindicates the event type, using the enumerations listed and described in Section 11.1.uEventis a structure containing the event data from the union of structures detailed in Section 8.2.2.2.
Parent topic:Event structures
ZPS_tuAfEventData#
This structure is a union of the data structures for the individual events described in Section 8.2.2.3 through to Section 8.2.2.25.
The ZPS_tuAfEventDatastructure is detailed below.
typedef union
{
ZPS_tsAfDataIndEvent sApsDataIndEvent;
ZPS_tsAfDataConfEvent sApsDataConfirmEvent;
ZPS_tsAfDataAckEvent sApsDataAckEvent;
ZPS_tsAfNwkFormationEvent sNwkFormationEvent;
ZPS_tsAfNwkJoinedEvent sNwkJoinedEvent;
ZPS_tsAfNwkJoinFailedEvent sNwkJoinFailedEvent;
ZPS_tsAfNwkDiscoveryEvent sNwkDiscoveryEvent;
ZPS_tsAfNwkJoinIndEvent sNwkJoinIndicationEvent;
ZPS_tsAfNwkLeaveIndEvent sNwkLeaveIndicationEvent;
ZPS_tsAfNwkLeaveConfEvent sNwkLeaveConfirmEvent;
ZPS_tsAfNwkStatusIndEvent sNwkStatusIndicationEvent;
ZPS_tsAfNwkRouteDiscoveryConfEvent sNwkRouteDiscoveryConfirmEvent;
ZPS_tsAfPollConfEvent sNwkPollConfirmEvent;
ZPS_tsAfNwkEdScanConfEvent sNwkEdScanConfirmEvent;
ZPS_tsAfErrorEvent sAfErrorEvent;
ZPS_tsAfZdoBindEvent sZdoBindEvent;
ZPS_tsAfZdoUnbindEvent sZdoUnbindEvent;
ZPS_tsAfZdoLinkKeyEvent sZdoLinkKeyEvent;
ZPS_tsAfBindRequestServerEvent sBindRequestServerEvent;
ZPS_tsAfInterPanDataIndEvent sApsInterPanDataIndEvent;
ZPS_tsAfInterPanDataConfEvent sApsInterPanDataConfirmEvent;
ZPS_tsAfZdpEvent sApsZdpEvent;
} ZPS_tuAfEventData;
Parent topic:Event structures
ZPS_tsAfDataIndEvent#
This structure is used in the ZPS_EVENT_APS_DATA_INDICATION event, which indicates the arrival of data on the local node.
The ZPS_tsAfDataIndEventstructure is detailed below.
typedef struct
{
uint8 u8DstAddrMode;
ZPS_tuAddress uDstAddress;
uint8 u8DstEndpoint;
uint8 u8SrcAddrMode;
ZPS_tuAddress uSrcAddress;
uint8 u8SrcEndpoint;
uint16 u16ProfileId;
uint16 u16ClusterId;
PDUM_thAPduInstance hAPduInst;
uint8 eStatus;
uint8 eSecurityStatus;
uint8 u8LinkQuality;
uint32 u32RxTime;
} ZPS_tsAfDataIndEvent;
where:
u8DstAddrModeindicates the type of destination address specified through the elementuDstAddress(see the Table below.)uDstAddressis the address of the destination node for the data packet (the type of address is specified using the elementu8DstAddrModeabove).u8DstEndpointis the number of the destination endpoint (in range 0-240).u8SrcAddrModeindicates the type of source address specified through the elementuSrcAddress(below) - this can be a 64-bit MAC/IEEE address or a 16-bit network address.uSrcAddressis the address of the source node for the data packet (the type of address is specified using the elementu8SrcAddrModeabove).u8SrcEndpointis the number of the source endpoint (in range 1-240).u16ProfileIdis the identifier of the ZigBee device profile of the device which can interpret the data.u16ClusterIdis the identifier of the cluster (which belongs to the device profile specified inu16ProfileId) which is capable of interpreting the data.hAPduInstis the handle of the APDU which contains the data.eStatusis one of the status codes from the NWK layer or MAC layer, detailed in Section 11.2.3 and Section 11.2.4.eSecurityStatusindicates the type of security with which the packet was sent. It can be: unsecured (0xAF), secured with network key (0xAC), or secured with link key (0xAB).u8LinkQualityis a measure of the signal strength of the radio link over which the data packet was sent (for the last hop).u32RxTimeis reserved for future use.
Addressing modes
u8DstAddrMode |
Code |
Description |
|---|---|---|
0x00 |
ZPS_E_ADDR_MODE_BOUND |
Bound endpoint |
0x01 |
ZPS_E_ADDR_MODE_GROUP |
16-bit Group address |
0x02 |
ZPS_E_ADDR_MODE_SHORT |
16-bit Network (Short) address |
0x03 |
ZPS_E_ADDR_MODE_IEEE |
64-bit IEEE/MAC address |
Parent topic:Event structures
ZPS_tsAfDataConfEvent#
This structure is used in the ZPS_EVENT_APS_DATA_CONFIRM event, which confirms that a data packet sent by the local node has been successfully passed down the stack to the MAC layer and has made its first hop toward its destination (an acknowledgment has been received from the next hop node).
The ZPS_tsAfDataConfEventstructure is detailed below.
typedef struct {
uint8 u8Status;
uint8 u8SrcEndpoint;
uint8 u8DstEndpoint;
uint8 u8DstAddrMode;
ZPS_tuAddress uDstAddr;
uint8 u8SequenceNum;
} ZPS_tsAfDataConfEvent;
where:
u8Statusis one of the status codes from the lower stack layers, detailed in Section 11.2.u8SrcEndpointis the number of the (local) source endpoint for the data transfer (in range 1-240).u8DstEndpointis the number of the destination endpoint for the data transfer (in range 1-240).u8DstAddrModeindicates the type of destination address specified through the elementuDstAddr(see Table) - only values 0x02 (group address) and 0x03 (network address) are valid in this structure.uDstAddris the address of the destination node for the data packet (the type of address is specified using the elementu8DstAddrModeabove).u8SequenceNumis the sequence number of the request that initiated the data transfer.
Parent topic:Event structures
ZPS_tsAfDataAckEvent#
This structure is used in the ZPS_EVENT_APS_DATA_ACK event, which is generated when an end-to-end acknowledgment is received from the destination node during a data transfer in which an acknowledgment was requested.
typedef struct {
uint8 u8Status;
uint8 u8SrcEndpoint;
uint8 u8DstEndpoint;
uint8 u8DstAddrMode;
uint16 u16DstAddr;
uint8 u8SequenceNum;
uint16 u16ProfileId;
uint16 u16ClusterId;
} ZPS_tsAfDataAckEvent;
where:
u8Statusis one of the status codes from the lower stack layers, detailed in Section 11.2.u8SrcEndpointis the number of the (local) source endpoint for the data transfer (in range 1-240).u8DstEndpointis the number of the destination endpoint for the data transfer (in range 1-240).u8DstAddrModeindicates the type of destination address specified through the elementu16DstAddr(see Table) - only values 0x01 (group address) and 0x02 (network address) are valid in this structure.u16DstAddris the 16-bit address of the destination node for the data transfer and therefore of the node that sent the acknowledgment (the type of address is specified using the elementu8DstAddrModeabove).u8SequenceNumis the sequence number of the request that initiated the data transfer.u16ProfileIdis the identifier of the ZigBee device profile of the device for which the data transfer was intended.u16ClusterIdis the identifier of the cluster (which belongs to the device profile specified inu16ProfileId) for which the data transfer was intended.
Parent topic:Event structures
ZPS_tsAfNwkFormationEvent#
This structure is used in the event ZPS_EVENT_NWK_STARTED, which indicates whether the network has been started (on the Coordinator).
The ZPS_tsAfNwkFormationEventstructure is detailed below.
typedef struct {
uint8 u8Status;
} ZPS_tsAfNwkFormationEvent;
where is one of the status codes from the lower stack layers, detailed in Section 11.2.
Parent topic:Event structures
ZPS_tsAfNwkJoinedEvent#
This structure is used in the events ZPS_EVENT_NWK_JOINED_AS_ROUTER and ZPS_EVENT_NWK_JOINED_AS_ENDDEVICE, which confirm that the local device (Router or End Device) has successfully joined a network.
The ZPS_tsAfNwkJoinedEventstructure reports the network address that the parent has assigned to the new node and is detailed below.
typedef struct
{
uint16 u16Addr;
bool_t bRejoin;
} ZPS_tsAfNwkJoinedEvent;
where:
u16Addris the 16-bit network address allocated to the joining node.bRejoinindicates whether the join was a rejoin (TRUE) or a new association (FALSE).
Parent topic:Event structures
ZPS_tsAfNwkJoinFailedEvent#
This structure is used in the event ZPS_EVENT_NWK_FAILED_TO_JOIN, which indicates that the local device has failed to join a network.
The ZPS_tsAfNwkJoinFailedEventstructure is detailed below.
typedef struct
{
uint8 u8Status;
bool_t bRejoin;
} ZPS_tsAfNwkJoinFailedEvent;
where:
u8Statusis one of the status codes from the lower stack layers, detailed in Section 11.2.bRejoinindicates whether the join attempt was a rejoin (TRUE) or a new association (FALSE).
Parent topic:Event structures
ZPS_tsAfNwkDiscoveryEvent#
This structure is used in the ZPS_EVENT_NWK_DISCOVERY_COMPLETE event, which reports the details of the networks detected in a network discovery initiated by a Router or End Device that needs to join a network.
The ZPS_tsAfNwkDiscoveryEventstructure is detailed below.
typedef struct
{
uint32 u32UnscannedChannels;
uint8 eStatus;
uint8 u8NetworkCount;
uint8 u8SelectedNetwork;
ZPS_tsNwkNetworkDescr *psNwkDescriptors;
} ZPS_tsAfNwkDiscoveryEvent;
where:
u32UnscannedChannelsis a 32-bit bitmap representing the set of channels from the network discovery that had not yet been scanned when this event was generated. Bits 11 to 26 represent the 2400-MHz channels 11 to 26, where 1 indicates channel scanned and 0 indicates channel not yet scanned.estatusis the status of the network discovery process, returned by the lower layers (see Section 11.2) - MAC_ENUM_SUCCESS, if the discovery was successfully completed.u8NetworkCountis the number of networks that had been discovered when this event was generated.u8SelectedNetworkis the index of the recommended network in the array of reported networks (see below).psNwkDescriptorsis a pointer to the network discovery table in the network NIB. The network discovery table contains an array of data structures, where each structure contains details of a discovered network. Each array element is a structure of the typeZPS_tsNwkNetworkDescr, described in Section 8.2.3.1. The number of array elements is given byu8NetworkCount, described above.
Parent topic:Event structures
ZPS_tsAfNwkJoinIndEvent#
This structure is used in the event ZPS_EVENT_NWK_NEW_NODE_HAS_JOINED, which notifies a Router or the Coordinator that a new child node has joined the network.
The ZPS_tsAfNwkJoinIndEventstructure contains information about the new node and is detailed below.
typedef struct
{
uint64 u64ExtAddr;
uint16 u16NwkAddr;
uint8 u8Capability;
uint8 u8Rejoin;
uint8 u8SecureRejoin;
} ZPS_tsAfNwkJoinIndEvent;
where:
u64ExtAddris the 64-bit IEEE (MAC) address of the joining node.u16NwkAddris the 16-bit network address assigned to the joining node.u8Capabilityis a bitmap indicating the operational capabilities of the joining node. This bitmap is detailed in Table below.u8Rejoinindicates the method used to join the network:0x00if joined through association.0x01if joined directly or used orphaning.0x02if was network rejoin.
u8SecureRejoinindicates whether the join was performed in a secure manner.zero represents FALSE.
a non-zero value represents TRUE.
Node capabilities bitmap
Bits |
Description |
|---|---|
0 |
Coordinator capability: |
1 |
Device type: |
2 |
Power source: |
3 |
Receiver on when idle: |
4-5 |
Reserved |
6 |
Security capability: |
7 |
Allocate address: |
Parent topic:Event structures
ZPS_tsAfNwkLeaveIndEvent#
This structure is used in the ZPS_EVENT_LEAVE_INDICATION event, which indicates that a neighboring node has left the network or a remote node has requested the local node to leave.
The ZPS_tsAfNwkLeaveIndEventstructure is detailed below.
typedef struct {
uint64 u64ExtAddr;
uint8 u8Rejoin;
} ZPS_tsAfNwkLeaveIndEvent;
where:
u64ExtAddris the 64-bit IEEE (MAC) address of the node that has left the network, or is zero if the local node has been requested to leave the networku8Rejoinindicates whether the leaving node was requested to attempt a subsequent rejoin of the network:zero represents FALSE
a non-zero value represents TRUE.
Parent topic:Event structures
ZPS_tsAfNwkLeaveConfEvent#
This structure is used in the event ZPS_EVENT_NWK_LEAVE_CONFIRM, which reports the results of a node leave request issued by the local node.
The ZPS_tsAfNwkLeaveConfEventstructure is detailed below.
typedef struct {
uint64 u64ExtAddr;
uint8 eStatus;
} ZPS_tsAfNwkLeaveConfEvent;
where:
u64ExtAddris the 64-bit IEEE (MAC) address of the leaving node. This value is zero if the local node itself is leaving.eStatusis the leave status returned by the lower layers - ZPS_NWK_ENUM_SUCCESS, if the leave request has been successful.
Parent topic:Event structures
ZPS_tsAfNwkStatusIndEvent#
This structure is used in the ZPS_EVENT_NWK_STATUS_INDICATION event, which reports status information from the NWK layer of the stack.
The ZPS_tsAfNwkStatusIndEventstructure is detailed below.
typedef struct {
uint16 u16NwkAddr;
uint8 u8Status;
} ZPS_tsAfNwkStatusIndEvent;
where:
u16NwkAddris the 16-bit network address of the node associated with the event.u8Statusis one of the status codes from the lower stack layers, detailed in Section 11.2.
Parent topic:Event structures
ZPS_tsAfNwkRouteDiscoveryConfEvent#
This structure is used in the ZPS_EVENT_NWK_ROUTE_DISCOVERY_CONFIRM event, which confirms that a route discovery has been performed.
The ZPS_tsAfNwkRouteDiscoveryConfEventstructure is detailed below.
typedef struct {
uint16 u16DstAddress;
uint8 u8Status;
uint8 u8NwkStatus;
} ZPS_tsAfNwkRouteDiscoveryConfEvent;
where:
u16DstAddressis the destination address for which the route discovery confirm event was generated.u8Statusis one of the status codes from the MAC layer, detailed in Section11.2.4.u8NwkStatusis one of the status codes from the NWK layer, detailed in Section 11.2.3.
Parent topic:Event structures
ZPS_tsAfPollConfEvent#
This structure is used in the ZPS_EVENT_NWK_POLL_CONFIRM event, which reports the completion of a poll request sent from the (local) End Device to its parent.
The ZPS_tsAfPollConfEventstructure is detailed below.
typedef struct {
uint8 u8Status;
} ZPS_tsAfPollConfEvent;
where u8Statusis one of the status codes from the lower stack layers, detailed in Section 11.2.
Parent topic:Event structures
ZPS_tsAfNwkEdScanConfEvent#
This structure is used in the ZPS_EVENT_NWK_ED_SCAN event, which indicates that an ‘energy detect’ scan in the 2.4-GHz radio band is completed.
The ZPS_tsAfNwkEdScanConfEventstructure is defined as:
typedef ZPS_tsNwkNlmeCfmEdScan ZPS_tsAfNwkEdScanConfEvent;
where ZPS_tsNwkNlmeCfmEdScanis described in Section 8.2.3.2.
Parent topic:Event structures
ZPS_tsAfErrorEvent#
This structure is used in the ZPS_EVENT_ERROR event, which reports error situations concerning the storage of received messages in APDU instances.
The ZPS_tsAfErrorEventstructure is detailed below.
typedef struct {
enum {
ZPS_ERROR_APDU_TOO_SMALL,
ZPS_ERROR_APDU_INSTANCES_EXHAUSTED,
ZPS_ERROR_NO_APDU_CONFIGURED,
ZPS_ERROR_OS_MESSAGE_QUEUE_OVERRUN
} eError;
union {
struct {
uint16 u16ProfileId;
uint16 u16ClusterId;
uint16 u16SrcAddr;
uint16 u16DataSize;
PDUM_thAPdu hAPdu;
uint8 u8SrcEndpoint;
uint8 u8DstEndpoint;
}sAfErrorApdu;
struct {
OS_thMessage hMessage;
} sAfErrorOsMessageOverrun;
} uErrorData;
} ZPS_tsAfErrorEvent;
The member enumerations and structures of the above structure are detailed below.
eError enumerations#
The error enumerations which are part of the ZPS_tsAfErrorEventstructure are listed and described below.
eError Enumerations
eError Enumeration |
Description |
|---|---|
ZPS_ERROR_APDU_TOO_SMALL |
Allocated APDU instance is too small to accommodate received message. This error is detailed in the structure |
ZPS_ERROR_APDU_INSTANCES_EXHAUSTED |
The are no APDU instances available to accommodate the received message. This error is detailed in the structure |
ZPS_ERROR_NO_APDU_CONFIGURED |
No APDU has been configured to accommodate the received message. This error is detailed in the structure |
ZPS_ERROR_OS_MESSAGE_QUEUE_OVERRUN |
A message queue is full and can accept no more messages. This error is detailed in the structure |
sAfErrorApdu
This structure is used in the following errors:
ZPS_ERROR_APDU_TOO_SMALL, which reports that the allocated APDU instance is too small to store a received message.
ZPS_ERROR_APDU_INSTANCES_EXHAUSTED, which reports that there are no allocated APDU instances left to store a received message.
ZPS_ERROR_NO_APDU_CONFIGURED, which reports that no APDU has been configured to store the received message.
The sAfErrorApdustructure is detailed below.
struct {
uint16 u16ProfileId;
uint16 u16ClusterId;
uint16 u16SrcAddr;
uint16 u16DataSize;
PDUM_thAPdu hAPdu;
uint8 u8SrcEndpoint;
uint8 u8DstEndpoint;
}sAfErrorApdu;
where:
u16ProfileIdis the identifier of the ZigBee application profile associated with the source and destination endpoints for the message.u16ClusterIdis the identifier of the cluster associated with the source and destination endpoints for the message.u16SrcAddris the 16-bit network address of the source node of the message.u16DataSizeis the size of the received message, in bytes.hAPduis the handle of the local APDU pool from which the APDU instance comes.u8SrcEndpointis the number of the source endpoint of the message.u8DstEndpointis the number of the destination endpoint of the message.
Parent topic:ZPS_tsAfErrorEvent
sAfErrorOsMessageOverrun#
This structure is used in the ZPS_ERROR_OS_MESSAGE_QUEUE_OVERRUN error, which indicates that a message queue is full and can accept no more messages.
The sAfErrorOsMessageOverrunstructure is detailed below.
struct {
OS_thMessage hMessage;
} sAfErrorOsMessageOverrun;
where hMessageis the handle of the message type for the queue which is full.
Parent topic:ZPS_tsAfErrorEvent
Parent topic:Event structures
ZPS_tsAfZdoBindEvent#
This structure is used in the ZPS_EVENT_ZDO_BIND event, which indicates that the local node has been successfully bound to one or more remote nodes.
The ZPS_tsAfZdoBindEventstructure is detailed below.
typedef struct { ZPS_tuAddress uDstAddr; uint8 u8DstAddrMode; uint8 u8SrcEp; uint8 u8DstEp; } ZPS_tsAfZdoBindEvent;
where
uDstAddris the address of the remote node for the binding (the type of address is specified using the elementu8DstAddrModeabove).u8DstAddrModeindicates the type of address specified through the elementuDstAddr(see Table 1).u8SrcEpis the number of the source endpoint for the binding (in range 1-240).u8DstEpis the number of the destination endpoint for the binding (in range 1-240).
Parent topic:Event structures
ZPS_tsAfZdoUnbindEvent#
This structure is used in the ZPS_EVENT_ZDO_UNBIND event, which indicates that the local node has been successfully unbound from one or more remote nodes.
The ZPS_tsAfZdoUnbindEventstructure is defined as:
typedef ZPS_tsAfZdoBindEvent ZPS_tsAfZdoUnbindEvent;
where ZPS_tsAfZdoBindEventis described in Section 8.2.2.18\ (but for this event, the data in the structure relates to unbinding rather than binding).
Parent topic:Event structures
ZPS_tsAfZdoLinkKeyEvent#
This structure is used in the ZPS_EVENT_ZDO_LINK_KEY event, which indicates that a new application link key has been received and installed, and is ready for use.
The ZPS_tsAfZdoLinkKeyEventstructure is defined as:
typedef struct {
uint64 u64IeeeLinkAddr;
} ZPS_tsAfZdoLinkKeyEvent;
where u64IeeeLinkAddris the IEEE/MAC address of the remote device with which the installed link key is valid.
Parent topic:Event structures
ZPS_tsAfBindRequestServerEvent#
This structure is used in the ZPS_EVENT_BIND_REQUEST_SERVER event, which reports the status of a data transmission sent from the (local) node to a set of bound endpoints.
The ZPS_tsAfBindRequestServerEventstructure is detailed below.
typedef struct {
uint8 u8Status;
uint8 u8SrcEndpoint;
uint32 u32FailureCount;
} ZPS_tsAfBindRequestServerEvent;
where:
u8Statusis the overall status of the bound data transmission:Success (0) indicates that the data packet was successfully transmitted to all bound endpoints
Failure (non-zero value) indicates that the data packet was not successfully sent to at least one bound endpoint (see
u32FailureCountbelow).
u8SrcEndpointis the number of the local endpoint from which the data packet was sent.u32FailureCountis the number of bound endpoints for which the transmission failed.
Parent topic:Event structures
ZPS_tsAfInterPanDataIndEvent#
This structure is used in the ZPS_EVENT_APS_INTERPAN_DATA_INDICATION event, which indicates that an inter-PAN data packet has arrived.
The ZPS_tsAfInterPanDataIndEventstructure is detailed below.
typedef struct
{
ZPS_tsInterPanAddress sDstAddr;
uint8 u8SrcAddrMode;
uint16 u16SrcPan;
uint64 u64SrcAddress;
uint16 u16ProfileId;
uint16 u16ClusterId;
PDUM_thAPduInstance hAPduInst;
uint8 eStatus;
uint8 u8DstEndpoint;
uint8 u8LinkQuality;
} ZPS_tsAfInterPanDataIndEvent;
where
sDstAddris a structure of the typeZPS_tsInterPanAddress(see Section8.2.3.3) which contains the PAN ID and address for the destination node(s) of the inter-PAN data packet.u8SrcAddrModeindicates the type of address specified through the elementu64SrcAddress(see Table).u16SrcPanis the PAN ID of the network from which the data packet originates.u64SrcAddressis the address of the node which sent the data packet (the type of address is specified using the elementu8SrcAddrModeabove).u16ProfileIdis the identifier of the application profile for which the data packet is intended.u16ClusterIdis the identifier of the cluster for which the data packet is intended.hAPduInstis the handle of the APDU instance for the data packet.eStatusis one of the status codes from the lower stack layers, detailed in Section 11.2.u8DstEndpointis the number of the destination endpoint for the data packet (in range 1-240).u8LinkQualityis an LQI value indicating the perceived strength of the radio signal which carried the received data packet.
Parent topic:Event structures
ZPS_tsAfInterPanDataConfEvent#
This structure is used in the ZPS_EVENT_APS_INTERPAN_DATA_CONFIRM event, which indicates that an inter-PAN communication has been sent by the local node and an acknowledgment has been received from the first hop node (this acknowledgment is not generated in the case of a broadcast).
The ZPS_tsAfInterPanDataConfEventstructure is detailed below.
typedef struct {
uint8 u8Status;
uint8 u8Handle;
} ZPS_tsAfInterPanDataConfEvent;
where
u8Statusis one of the status codes from the lower stack layers, detailed in Section 11.2.u8Handleis a handle for internal use.
Parent topic:Event structures
ZPS_tsAfTCstatusEvent#
This structure is used in the ZPS_EVENT_TC_STATUS event, which indicates whether negotiations to establish a link key with the Trust Centre have been successful and, if so, which key is the active key.
The ZPS_tsAfTCstatusEventstructure is detailed below.
typedef struct
{
ZPS_tuTcStatusData uTcData;
uint8 u8Status;
}ZPS_tsAfTCstatusEvent;
where:
uTcDatais dependent onu8Status(below) and is either a pointer to the link key descriptor in the case of success or the address of the Trust Centre node in the case of failure.ZPS_tuTcStatusDatais a union, detailed below.u8Statusindicates the results of the link key negotiations - one of:ZPS_E_SUCCESS (link key successfully established)
ZPS_APL_APS_E_SECURITY_FAIL (link key not established)
The ZPS_tuTcStatusDatastructure is detailed below.
typedef union {
ZPS_tsAplApsKeyDescriptorEntry *pKeyDesc;
uint64 u64ExtendedAddress;
} PS_tuTcStatusData;
where:
pKeyDescis a pointer to the active link key, if successfully established, which is contained in the structure described in Section 8.2.3.6.u64ExtendedAddressis the IEEE/MAC address of the Trust Centre node with which link key negotiations failed.
Parent topic:Event structures
ZPS_tsAfZdpEvent#
This structure is used when a ZPS_EVENT_APS_DATA_INDICATION event is generated containing a response which is destined for the ZDO at endpoint 0. The application can extract the response data from the event using the function ZPS_bAplZdpUnpackResponse() and this structure is used to receive the extracted data.
The ZPS_tsAfZdpEventstructure is detailed below.
typedef struct {
uint8 u8SequNumber;
uint16 u16ClusterId;
union {
ZPS_tsAplZdpDeviceAnnceReq sDeviceAnnce;
ZPS_tsAplZdpMgmtNwkUpdateReq sMgmtNwkUpdateReq;
ZPS_tsAplZdpMgmtPermitJoiningReq sPermitJoiningReq;
ZPS_tsAplZdpDiscoveryCacheRsp sDiscoveryCacheRsp;
ZPS_tsAplZdpDiscoveryStoreRsp sDiscoveryStoreRsp;
ZPS_tsAplZdpNodeDescStoreRsp sNodeDescStoreRsp;
ZPS_tsAplZdpActiveEpStoreRsp sActiveEpStoreRsp;
ZPS_tsAplZdpSimpleDescStoreRsp sSimpleDescStoreRsp;
ZPS_tsAplZdpRemoveNodeCacheRsp sRemoveNodeCacheRsp;
ZPS_tsAplZdpEndDeviceBindRsp sEndDeviceBindRsp;
ZPS_tsAplZdpBindRsp sBindRsp;
ZPS_tsAplZdpUnbindRsp sUnbindRsp;
ZPS_tsAplZdpReplaceDeviceRsp sReplaceDeviceRsp;
ZPS_tsAplZdpStoreBkupBindEntryRsp sStoreBkupBindEntryRsp;
ZPS_tsAplZdpRemoveBkupBindEntryRsp sRemoveBkupBindEntryRsp;
ZPS_tsAplZdpBackupSourceBindRsp sBackupSourceBindRsp;
ZPS_tsAplZdpMgmtLeaveRsp sMgmtLeaveRsp;
ZPS_tsAplZdpMgmtDirectJoinRsp sMgmtDirectJoinRsp;
ZPS_tsAplZdpMgmtPermitJoiningRsp sPermitJoiningRsp;
ZPS_tsAplZdpNodeDescRsp sNodeDescRsp;
ZPS_tsAplZdpPowerDescRsp sPowerDescRsp;
ZPS_tsAplZdpSimpleDescRsp sSimpleDescRsp;
ZPS_tsAplZdpNwkAddrRsp sNwkAddrRsp;
ZPS_tsAplZdpIeeeAddrRsp sIeeeAddrRsp;
ZPS_tsAplZdpUserDescConf sUserDescConf;
ZPS_tsAplZdpSystemServerDiscoveryRsp sSystemServerDiscoveryRsp;
ZPS_tsAplZdpPowerDescStoreRsp sPowerDescStoreRsp;
ZPS_tsAplZdpUserDescRsp sUserDescRsp;
ZPS_tsAplZdpActiveEpRsp sActiveEpRsp;
ZPS_tsAplZdpMatchDescRsp sMatchDescRsp;
ZPS_tsAplZdpComplexDescRsp sComplexDescRsp;
ZPS_tsAplZdpFindNodeCacheRsp sFindNodeCacheRsp;
ZPS_tsAplZdpExtendedSimpleDescRsp sExtendedSimpleDescRsp;
ZPS_tsAplZdpExtendedActiveEpRsp sExtendedActiveEpRsp;
ZPS_tsAplZdpBindRegisterRsp sBindRegisterRsp;
ZPS_tsAplZdpBackupBindTableRsp sBackupBindTableRsp;
ZPS_tsAplZdpRecoverBindTableRsp sRecoverBindTableRsp;
ZPS_tsAplZdpRecoverSourceBindRsp sRecoverSourceBindRsp;
ZPS_tsAplZdpMgmtNwkDiscRsp sMgmtNwkDiscRsp;
ZPS_tsAplZdpMgmtLqiRsp sMgmtLqiRsp;
ZPS_tsAplZdpMgmtRtgRsp sRtgRsp;
ZPS_tsAplZdpMgmtBindRsp sMgmtBindRsp;
ZPS_tsAplZdpMgmtCacheRsp sMgmtCacheRsp;
ZPS_tsAplZdpMgmtNwkUpdateNotify sMgmtNwkUpdateNotify;
}uZdpData;
union {
ZPS_tsAplZdpBindingTableEntry asBindingTable[5];
ZPS_tsAplZdpNetworkDescr asNwkDescTable[5];
ZPS_tsAplZdpNtListEntry asNtList[2];
ZPS_tsAplDiscoveryCache aDiscCache[5];
uint16 au16Data[34];
uint8 au8Data[77];
uint64 au64Data[9];
}uLists;
}ZPS_tsAfZdpEvent;
where:
u8SequNumberis the sequence number of the ZDP request/responseu16ClusterIdis the ID of the cluster to which the request/response relatesuZdpDatais a union of the different ZDP request/response types:sDeviceAnnceis a structure of the typeZPS_tsAplZdpDeviceAnnceReq, described in Section 9.2.2.3
sMgmtNwkUpdateReqis a structure of the typeZPS_tsAplZdpMgmtNwkUpdateReq, described in Section 9.2.2.41sPermitJoiningReqis a structure of the typeZPS_tsAplZdpMgmtPermitJoiningReq, described in Section 9.2.3.39sDiscoveryCacheRspis a structure of the typeZPS_tsAplZdpDiscoveryCacheRsp, described in Section 9.2.3.14sDiscoveryStoreRspis a structure of the typeZPS_tsAplZdpDiscoveryStoreRsp, described in Section 9.2.3.15sNodeDescStoreRspis a structure of the typeZPS_tsAplZdpNodeDescStoreRsp, described in Section 9.2.3.16sActiveEpStoreRspis a structure of the typeZPS_tsAplZdpActiveEpStoreRsp, described in Section 9.2.3.19sSimpleDescStoreRspis a structure of the typeZPS_tsAplZdpSimpleDescStoreRsp, described in Section 9.2.3.18sRemoveNodeCacheRspis a structure of the typeZPS_tsAplZdpRemoveNodeCacheRsp, described in Section 9.2.3.21sEndDeviceBindRspis a structure of the typeZPS_tsAplZdpEndDeviceBindRsp, described in Section 9.2.3.22sBindRspis a structure of the typeZPS_tsAplZdpBindRsp, described in Section 9.2.3.23sUnbindRspis a structure of the typeZPS_tsAplZdpUnbindRsp, described in Section 9.2.3.24sReplaceDeviceRspis a structure of the typeZPS_tsAplZdpReplaceDeviceRsp, described in Section 9.2.3.26sStoreBkupBindEntryRspis a structure of the typeZPS_tsAplZdpStoreBkupBindEntryRsp, described in Section9.2.2.27sRemoveBkupBindEntryRspis a structure of the typeZPS_tsAplZdpRemoveBkupBindEntryRsp, described in Section9.2.2.28sBackupSourceBindRspis a structure of the typeZPS_tsAplZdpBackupSourceBindRsp, described in Section 9.2.3.31sMgmtLeaveRspis a structure of the typeZPS_tsAplZdpMgmtLeaveRsp, described in Section 9.2.3.37sMgmtDirectJoinRspis a structure of the typeZPS_tsAplZdpMgmtDirectJoinRsp, described in Section 9.2.3.38sPermitJoiningRspis a structure of the typeZPS_tsAplZdpMgmtPermitJoiningRsp, described in Section 9.2.3.39sNodeDescRspis a structure of the typeZPS_tsAplZdpNodeDescRsp, described in Section 8.2.3.3sPowerDescRspis a structure of the typeZPS_tsAplZdpPowerDescRsp, described in Section 9.2.3.4sSimpleDescRspis a structure of the typeZPS_tsAplZdpSimpleDescRsp, described in Section 9.2.3.5sNwkAddrRspis a structure of the typeZPS_tsAplZdpNwkAddrRsp, described in Section 9.2.3.1sIeeeAddrRspis a structure of the typeZPS_tsAplZdpIeeeAddrRsp, described in Section 9.2.3.2sUserDescConfis a structure of the typeZPS_tsAplZdpUserDescConf, described in Section 9.2.3.12sSystemServerDiscoveryRspis a structure of the typeZPS_tsAplZdpSystemServerDiscoveryRsp, described in Section9.2.3.13sPowerDescStoreRspis a structure of the typeZPS_tsAplZdpPowerDescStoreRsp, described in Section 9.2.3.17sUserDescRspis a structure of the typeZPS_tsAplZdpUserDescRsp, described in Section 9.2.3.8sActiveEpRspis a structure of the typeZPS_tsAplZdpActiveEpRsp, described in Section 9.2.3.10sMatchDescRspis a structure of the typeZPS_tsAplZdpMatchDescRsp, described in Section 9.2.3.9sComplexDescRspis a structure of the typeZPS_tsAplZdpComplexDescRsp, described in Section 9.2.3.7sFindNodeCacheRspis a structure of the typeZPS_tsAplZdpFindNodeCacheRsp, described in Section 9.2.3.20sExtendedSimpleDescRspis a structure of the typeZPS_tsAplZdpExtendedSimpleDescRsp, described in Section 9.2.3.6sExtendedActiveEpRspis a structure of the typeZPS_tsAplZdpExtendedActiveEpRsp, described in Section 9.2.3.11sBindRegisterRspis a structure of the typeZPS_tsAplZdpBindRegisterRsp, described in Section 9.2.3.25sBackupBindTableRspis a structure of the typeZPS_tsAplZdpBackupBindTableRsp, described in Section 9.2.3.29sRecoverBindTableRspis a structure of the typeZPS_tsAplZdpRecoverBindTableRsp, described in Section 9.2.3.30sRecoverSourceBindRspis a structure of the typeZPS_tsAplZdpRecoverSourceBindRsp, described in Section 9.2.3.32sMgmtNwkDiscRspis a structure of the typeZPS_tsAplZdpMgmtNwkDiscRsp, described in Section 9.2.3.33sMgmtLqiRspis a structure of the typeZPS_tsAplZdpMgmtLqiRsp, described in Section 9.2.3.34sRtgRspis a structure of the typeZPS_tsAplZdpMgmtRtgRsp, described in Section 9.2.3.35sMgmtBindRspis a structure of the typeZPS_tsAplZdpMgmtBindRsp, described in Section 9.2.3.36sMgmtCacheRspis a structure of the typeZPS_tsAplZdpMgmtCacheRsp, described in Section 9.2.3.40sMgmtNwkUpdateNotifyis a structure of the typeZPS_tsAplZdpMgmtNwkUpdateNotify, described in Section 9.2.3.41uListsis a union of the different arrays/tables which act as temporary storage for data elements used by the stack (and are therefore for internal use only)
Parent topic:Event structures
Parent topic:AF structures
Other structures#
This section describes various structures used by the AF API. The structures are listed below.
ZPS_tsNwkNetworkDescr#
This structure is used in an array element in the structure ZPS_tsAfNwkDiscoveryEvent, which is created as part of the ZPS_EVENT_NWK_DISCOVERY_COMPLETE event. This event reports the networks detected during a network discovery (see Section 8.2.2.9).
The ZPS_tsNwkNetworkDescrstructure contains information on a detected network and is detailed below.
typedef struct
{
uint64 u64ExtPanId;
uint8 u8LogicalChan;
uint8 u8StackProfile;
uint8 u8ZigBeeVersion;
uint8 u8PermitJoining;
uint8 u8RouterCapacity;
uint8 u8EndDeviceCapacity;
} ZPS_tsNwkNetworkDescr;
where:
u64ExtPanIdis the Extended PAN ID of the discovered network.u8LogicalChanis the 2400-MHz channel on which the network was found.u8StackProfileis the Stack Profile of the discovered network:0 - manufacturer-specific
1 - ZigBee
2 - ZigBee PRO
other values reserved, and is fixed at 2 for the NXP stack
u8ZigBeeVersionis the ZigBee version of the discovered network.u8PermitJoiningindicates the number of detected nodes with ‘permit joining’ enabled (and therefore allowing nodes to join the network through them).u8RouterCapacityindicates the number of detected nodes that are allowing Routers to join the network through them.u8EndDeviceCapacityindicates the number of detected nodes that are allowing End Devices to join the network through them.
Parent topic:Other structures
ZPS_tsNwkNlmeCfmEdScan#
This structure is used by the structure ZPS_tsAfNwkEdScanConfEvent, which is created as part of the ZPS_EVENT_NWK_ED_SCAN event which reports the results of an ‘energy detect’ scan in the 2.4-GHz radio band.
The ZPS_tsNwkNlmeCfmEdScantstructure is detailed below.
typedef struct
{
uint8 u8Status;
uint8 u8ResultListSize;
uint8 au8EnergyDetect[ZPS_NWK_MAX_ED_RESULTS];
} ZPS_tsNwkNlmeCfmEdScan;
where
u8Statusis one of the status codes from the lower stack layers, detailed in Section 11.2.u8ResultListSizeis the number of entries in the results list (see below).au8EnergyDetect[]is an array containing the list of results of the energy scan (8-bit values representing the detected energy levels in the channels). There is one array element for each channel scanned, where element 0 is for the first channel scanned, element 1 is for the second channel scanned, etc.
Parent topic:Other structures
ZPS_tsInterPanAddress#
This structure is used to specify the destination for an inter-PAN transmission. The ZPS_tsInterPanAddressstructure is detailed below.
typedef struct
{
enum {
ZPS_E_AM_INTERPAN_GROUP = 0x01,
ZPS_E_AM_INTERPAN_SHORT,
ZPS_E_AM_INTERPAN_IEEE
}eMode;
uint16 u16PanId;
ZPS_tuAddress uAddress;
} ZPS_tsInterPanAddress;
where:
eModeis used to specify the type of destination address that will be used in the fielduAddressbelow. One of the following enumerations must be specified:ZPS_E_AM_INTERPAN_GROUPindicates that a 16-bit group address will be used to specify multiple target nodes in the destination network (the group address must be valid in the destination network)ZPS_E_AM_INTERPAN_SHORTindicates that a 16-bit network/short address will be used to specify a single target node or a broadcast to all nodes in the destination networkZPS_E_AM_INTERPAN_IEEEindicates that a 64-bit IEEE/MAC address will be used to specify a single target node in the destination network
u16PanIdis the PAN ID of the destination network - a value 0xFFFF can be used to specify a broadcast to all reachable ZigBee PRO networksuAddressis the address of the target node(s) in the destination network (the address type must be as specified above in theeModefield) - a value of 0xFFFF can be used to specify a broadcast to all nodes in the destination network(s).
Parent topic:Other structures
ZPS_tsAfProfileDataReq#
This structure is used to specify the transmission details for a data transmission submitted using the function ZPS_eAplAfApsdeDataReq().
The ZPS_tsAfProfileDataReqstructure is detailed below.
typedef struct {
ZPS_tuAddress uDstAddr;
uint16 u16ClusterId;
uint16 u16ProfileId;
uint8 u8SrcEp;
ZPS_teAplApsdeAddressMode eDstAddrMode;
uint8 u8DstEp;
ZPS_teAplAfSecurityMode eSecurityMode;
uint8 u8Radius;
}ZPS_tsAfProfileDataReq;
where:
uDstAddris the address of the destination node for the transmission request (can be 16- or 64-bit, as specified byeDstAddrMode).u16ClusterIdis the Cluster ID of the destination cluster.u16ProfileIdis the Profile ID of the destination application profile.u8SrcEpis the source endpoint number (1-240) on the local node.eDstAddrModeis the type of destination address, one of (also see the table, Table):ZPS_E_ADDR_MODE_BOUND (no address needed for bound nodes).
ZPS_E_ADDR_MODE_GROUP (16-bit group address).
ZPS_E_ADDR_MODE_SHORT (16-bit network address).
ZPS_E_ADDR_MODE_IEEE (64-bit IEEE/MAC address).
u8DstEpis the destination endpoint number (1-240) on the remote node.eSecurityModeis the security mode for the data transfer, one of:ZPS_E_APL_AF_UNSECURE (no security enabled)
ZPS_E_APL_AF_SECURE (Application-level security using link key and network key)
ZPS_E_APL_AF_SECURE_NWK (Network-level security using network key)
ZPS_E_APL_AF_SECURE | ZPS_E_APL_AF_EXT_NONCE (Application-level security using link key and network key with the extended NONCE included in the frame)
ZPS_E_APL_AF_WILD_PROFILE (May be combined with the above flags using OR operator. Sends the message using the wildcard profile (0xFFFF) instead of the profile in the associated Simple descriptor).
u8Radiusis the maximum number of hops permitted to the destination node (zero value specifies that default maximum is to be used).
Parent topic:Other structures
tsBeaconFilterType#
This structure contains the details of a beacon filter that can be introduced using the function ZPS_bAppAddBeaconFilter().
The tsBeaconFilterTypestructure is detailed below.
typedef struct
{
uint64 *pu64ExtendPanIdList;
uint16 u16Panid;
uint16 u16FilterMap;
uint8 u8ListSize;
uint8 u8Lqi;
uint8 u8Depth;
} tsBeaconFilterType;
where:
pu64ExtendPanIdListis a pointer to a list of 64-bit Extended PAN IDs (EPIDs) which acts as a blacklist or whitelist of networks, depending on the settings of bits 0 and 1 in theu8FilterMapbitmap:If this is a blacklist, beacons from networks with EPIDs in the list will not be accepted
If this is a whitelist, only beacons from networks with EPIDs in the list will be accepted
u16Panidis a 16-bit PAN ID on which beacons can be filteredu8ListSizeis the number of Extended PAN IDs in the list pointed to by
pu64ExtendPanIdList
u8Lqiis the minimum LQI value (in the range 0 to 255) of an acceptable beacon (any beacon with LQI value less than this minimum will be filtered out) - if required, this field must be enabled through bit 2 in theu8FilterMapbitmapu8Depthis the tree depth of the neighbor device. A value of 0x00 indicates that the device is the ZigBee coordinator for the network.u16FilterMapis an 16-bit bitmap detailing the filtering requirements, as follows:
Bit |
Enumeration |
Description |
|---|---|---|
0 |
BF_BITMAP_BLACKLIST(0x1) |
If set, field |
1 |
BF_BITMAP_WHITELIST (0x2) |
If set, field |
2 |
BF_BITMAP_LQI (0x4) |
If set, beacons must be filtered according to LQI value using the minimum in field |
3 |
BF_BITMAP_CAP_ENDDEVICE (0x8) |
If set, beacons from nodes with capacity for End Device children can be accepted. |
4 |
BF_BITMAP_CAP_ROUTER (0x10) |
If set, beacons from nodes with capacity for Router children can be accepted. |
5 |
BF_BITMAP_PERMIT_JOIN (0x20) |
If set, beacons from nodes with ‘permit join- ing’ enabled can be accepted. |
6 |
BF_BITMAP_SHORT_PAN (0x40) |
If set, beacons from nodes on a network with the PAN ID in |
7 |
- |
Reserved. |
8 |
BF_BITMAP_DEPTH |
If set, beacons from nodes on a network with the depth in u8Depth. if it is set to 0xff - filters out any beacon which is not from the coordinator. Any other value of u8Depth, filters out beacons with greater than or equal to |
Note: Bits 0 and 1 must not both be set.
Note: After each discovery or rejoin, the flags contained in the u16FilterMap field are cleared, while all other fields of this structure remain intact.
Parent topic:Other structures
ZPS_tsAplApsKeyDescriptorEntry#
This structure contains a link key for secured communications with another node.
typedef struct
{
uint32 u32OutgoingFrameCounter;
uint16 u16ExtAddrLkup;
uint8 au8LinkKey[ZPS_SEC_KEY_LENGTH];
} ZPS_tsAplApsKeyDescriptorEntry;
where:
u32OutgoingFrameCounteris the outgoing frame counter value which is incremented on each transmission to a destination address below.u16ExtAddrLkupis the index of the local look-up table entry that contains the IEEE/MAC address of either the Trust Centre or the target node.au8LinkKey[]is an array containing the link key.
Parent topic:Other structures
ZPS_tsAftsStartParamsDistributed#
This structure contains the start parameter values for a node in a distributed security network.
typedef struct
{
uint64 u64ExtPanId;
uint8 *pu8NwkKey;
uint16 u16PanId;
uint16 u16NwkAddr;
uint8 u8KeyIndex;
uint8 u8LogicalChannel;
uint8 u8NwkupdateId;
} ZPS_tsAftsStartParamsDistributed;
where:
u64ExtPanIdis the Extended PAN ID of the distributed security network.pu8NwkKeyis a pointer to a location to receive the network key.u16PanIdis the PAN ID of the network.u16NwkAddris the network address of the local node.u8KeyIndexis the sequence number required to identify the network key in the security set.u8LogicalChannelis the number of the radio channel on which the network operates.u8NwkupdateIdis a unique byte value which is incremented when the network parameters are updated (and is therefore used to determine whether a receiving node has missed an update).
Parent topic:Other structures
ZPS_tsAfFlashInfoSet#
This structure contains information about the devices Flash memory sector used for the persistent storage of unique link keys on the Trust Centre, as enabled by the function ZPS_vTcInitFlash().
typedef struct
{
uint16 u16SectorSize;
uint16 u16CredNodesCount;
uint8 u8SectorSet;
} ZPS_tsAfFlashInfoSet;
where:
u16SectorSizeis the size, in bytes, of the Flash memory sector used to store the link keys.u16CredNodesCountis the maximum number of nodes for which link keys can be stored in the Flash memory sector.u8SectorSetis the number of the Flash memory sector used for this storage.
Note: Care should be taken that this sector is set greater than the current flash usage of the image you are running. If this clashes with something else (image or user data), it would lead to flash corruption and the behavior might become non-deterministic.
Parent topic:Other structures
ZPS_TclkDescriptorEntry#
This structure is used on the Trust Centre to hold information in RAM about a link key for a node, where this link key is held in persistent storage in devices Flash memory, as enabled by the function ZPS_vTcInitFlash(). If this feature is used, the application must allocate space for an array of these structures in RAM, with one structure for each potential node in the network.
typedef struct
{
uint16 u16CredOffset;
uint16 u16TclkRetries;
} ZPS_TclkDescriptorEntry;
where:
u16CredOffsetis the offset, in bytes, of the storage location for the node’s link key in the relevant Flash memory sector.u16TclkRetriesis the number of retries that were attempted to negotiate the link key between the Trust Centre and the node.
Parent topic:Other structures
Parent topic:AF structures
Parent topic:Application Framework (AF) API